Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of My Conve, With Blister Pack

My Conve, With Blister Pack
Sales Price: 10.99 SGD
Review Rating: 2.33
3 Customer Reviews
5 star 0
4 star 1
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Material measurement at work
2
From Japan
On 2017-07-13 09:19:50
I used it for about a year. It is sometimes rather than everyday. Although the lock mechanism was easy to use, it is scary because the take-up speed is too fast. At the end the nail of the tip gave off. Design and size were also good, but it is disappointing.
This review is about item#5862762.
To measure internal law
1
From Japan
On 2014-01-30 13:26:02
I bought it to measure internal law, but just because the case is only 70mm graduation is normal, read the graduation from the case one by one, since you have to add another 70mm yourself, so bother There is no point in using. Moreover, the scale changes easily several millimeters depending on the viewpoint, and there is no solid lock mechanism only with the simple brake, so if you extend and shrink it before reading it, even if you read back to read it, it will be misaligned There is that. If you purchase it by trusting the Tajima brand while hoping for specifications exclusively for internal law that have a window on the case like a competitor and you can read the numbers of the best, it will fail. It is only a thing called "compact convex" to the last.
This review is about item#05862762.
Measurement of instrument dimensions for sketch drawing at work etc.
4
From Japan
On 2011-02-22 14:02:34
Tape width 13 mm is not obstructive and very easy to use. Since it is thin, putting it in your pocket does not matter.
This review is about item#05862762.
1
Customer Who Viewed This Item Also Viewed
Measure Tape
Tape Measure
Tape Measure 3.5m
Driver Cutter L500