Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pentagon Type Knob Bolt

Pentagon Type Knob Bolt
Sales Price: 10.99 SGD
Review Rating: 4.75
4 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Fixing the fence of the trimmer table
5
From Japan
On 2017-07-26 20:20:00
When making the trimmer table, I made the fence slidable, but I could easily fix it and wanted to be able to relax easily, so I was looking for a bolt that I could handle. The size of the knob was also large and I was able to get the result as intended.
This review is about item#3686094.
Tighten screws
4
From Japan
On 2017-06-21 06:25:23
It is saved for screw tightening in a place where a tool is necessary or where a tool can not be used. I want a long bolt extension product
This review is about item#03686121.
For fixing of combine covers
5
From Japan
On 2015-07-17 22:31:20
I want the length to be aligned in units of 5 mm
This review is about item#03686137.
OHASHI It is used as a spare for replacing the height adjustment screw of the music stand.
5
From Japan
On 2013-08-22 20:15:25
Manufacturer's genuine screws are also sold as expendable parts, but the unit price will change cheaper than that. As for the size of the knob and about the size of the knob, it was hard to find something of a good size just as if it was a manufacturer genuine, but finally finding this good product of a good size, exchanging parts in fact, try genuine I was able to use it in the same way as it was very good.
This review is about item#03686121.
1
Customer Who Viewed This Item Also Viewed
Seven Lob Knob, - External Thread Made From Steel-- M5
Clamping Lever
Plastic Cross-Joint Knob
Plastic Lobe Knob
Star Knob
Grill Knobs
Mom pot
  • Mom pot
  • YAMAZAKI (CONDOR)
  • 139.99 SGD
Seven Lob Knob Stainless Steel External Thread
Fit Knob, Black
Fit Knob, White
Lobe Knob Bolt