Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 13mm Stainless Double Ring

13mm Stainless Double Ring
Sales Price: 3.99 SGD
Review Rating: 3.71
7 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Tidy of key holders
4
From Japan
On 2017-07-20 08:56:14
Because it is small and solid, handling of keys is also good, and there is no need to worry about losing.
This review is about item#03550696.
Fixture supplement
5
From Japan
On 2017-05-23 14:50:15
Purchased as part of key ring. Because it is made of stainless steel, there is no need to worry about rust. I will repeat if I manage to do something a little more costly.
This review is about item#3550696.
Accessories
1
From Japan
On 2016-01-20 19:33:13
Although the inside diameter is 16 mm in the description of item, it is actually 17 mm. I wanted replacement because the item I wanted is 16 mm, but I was not able to do so because I ordered it. I want you to display it in actual item in actual size.
This review is about item#03550757.
Use as a key holder
2
From Japan
On 2014-04-30 17:16:06
Although it is described as 25 mm, the actual thing is 30 mm, it is huge
This review is about item#03550827.
To connect the lid of the bath with the chain
5
From Japan
On 2014-01-17 13:05:14
I am relieved with a strong product, so it is the previous repeater. I also want to place an order.
This review is about item#03550775.
Decorative curtain hanging
5
From Japan
On 2013-11-28 17:56:37
It was very easy to use.
This review is about item#03550757.
Mounting of suspended curtain
4
From Japan
On 2013-10-04 10:51:37
I am satisfied with building very firmly. But it is "hard" for that reason. It is hard anyhow. You can not let things pass unless you can open it with a flathead screwdriver. The difficulty is that it takes time to deliver. You have to order here with room.
This review is about item#03550836.
1
Customer Who Viewed This Item Also Viewed
Keyring
Double Ring in Plastic Case
Double Ring
Split Ring, Stainless Steel
Stainless Steel O-Rings
Stainless Ring
Double Link, Stainless Steel
Key Ring, Steel
Double Ring
Split Rings
Double Coil
W Ring, Double Ring
Chrome double ring
Ring (made of stainless steel)