Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stainless Ring

Stainless Ring
Sales Price: 1.99 SGD
Review Rating: 3.50
6 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Intangible cultural property designated by the city, inner stick decorations of Kimono Rice Dance
From Japan
On 2018-03-13 16:55:30
I appreciate quick delivery. I am really grateful if it arrives like this.
This review is about item#3552421.
As part of car accessories
From Japan
On 2018-01-11 17:07:31
Especially, there is no problem, the size is just right and it is good so that the size was planned for the attachment part.
This review is about item#3552412.
For roof-top shading net
From Japan
On 2017-12-10 15:46:29
It uses the stainless steel wire to open and close the light shielding net on the roof, but it is slippery, it is easy to open and close smoothly and easy to use.
This review is about item#3552403.
As a part.
From Japan
On 2016-12-27 10:01:57
I bought two inside diameter 38 mm, but actually it was 40 mm inside diameter and 42 mm inside diameter. Those who were 40 mm could use it, but 42 mm can not be used as expected.
This review is about item#3552437.
One pole tent
From Japan
On 2016-12-13 14:33:35
Use it as part to pass the peg through the hem belt of one pole tent. Previously used, it was pulled when the tent shrank due to dew condensation and night dew, and the metal fittings were bent, so we chose by strength emphasis. I think that it is strong against rust and is a good product with SUS 316.
This review is about item#3552403.
Used for hanging the whiteboard
From Japan
On 2014-08-06 14:19:48
It is written that the inside diameter is 38 mm, in fact it was 40 mm.
This review is about item#03552437.
Customer Who Viewed This Item Also Viewed
Round Link
Round Link, Stainless Steel
Round Ring
Stainless Steel O-Rings
Stainless Steel Ring
Round link
Round link
Round link
Ring (made of stainless steel)
Round link