Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of 6x1.25, Straight, Grease Nipple

6x1.25, Straight, Grease Nipple
Sales Price: 16.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 3
4 star 0
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Grease up
5
From Japan
On 2017-07-07 15:16:00
Since it is installed in the rotating part, it is necessary to exchange regularly, but this product is inexpensive and easy to obtain.
This review is about item#03723352.
Grease coating of shaft
3
From Japan
On 2015-10-25 21:22:19
it is normal.
This review is about item#03723352.
Mower grass headgear
5
From Japan
On 2015-09-04 08:17:14
Used for Kyoritsu's grass cutter. I removed the bolt and injected grease, but I greased up with grease gun. Grease up is painful as well! There are models that do not match with other manufacturers, so be careful.
This review is about item#03723352.
Maintenance of agricultural machines
3
From Japan
On 2013-12-10 17:22:22
I was troubled with a tap of a size not available in nearby mass merchandisers, but I could find it with monotaro and I did not have to purchase a machine shop high. However, because the tap was too long and the grease did not go in, we put two washers of stain and solved it. (It was a mistake when the spring and the ball jumped out when I tried to scrape the tap part at the beginning with the grinder and make a mistake.) Now it is perfect.
This review is about item#03723352.
Lubrication of the gear part of the harvester
5
From Japan
On 2013-06-07 08:24:43
The nipple of the millimeter thread standard was not readily available on the market, and it was using the inch standard to remodel it. It was very helpful to find this product.
This review is about item#03723352.
1