Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Grommet Punch Set

Grommet Punch Set
Sales Price: 45.99 SGD
Review Rating: 3.60
5 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
To add eyelets for tents.
1
From Japan
On 2017-06-27 20:13:41
Hatome punch which is attached does not have strength and it turns immediately. I do not know if usage is bad, but the eyelet can not be crushed well. Feeling that I bought and failed
This review is about item#3503342.
Rope stop of boat seat
4
From Japan
On 2017-05-07 17:39:54
It is in a case so it's convenient to carry and can be used effectively
This review is about item#3503367.
To a camper
5
From Japan
On 2017-04-17 06:44:56
Use it just as you attach a flexible solar cell to the upper part of the bank bed of the camper.
This review is about item#03503342.
Seat eyelet
5
From Japan
On 2016-08-15 22:37:37
I used a 12 mm diameter eyelet, but since the diameter was a little big, I purchased 10 mm. In addition, it is convenient because it is a set of three kinds of aluminum, brass, stainless steel.
This review is about item#3503342.
Repair of truck seat
3
From Japan
On 2015-06-03 16:02:35
There is a thing that it does not stop stopping properly.
This review is about item#03503367.
1
Customer Who Viewed This Item Also Viewed
Double-Sided Eyelet Punch
12mm Eyelet Punch
5&7mm Eyelet Punch
8mm Eyelet Punch
Both Sides Eyelet
Double-Sided Eyelet For Cast Rod
Punch Unit
Eyelet Punch Set
Hatomepanchi
Stainless Eyelet
Dedicated Hatomekoma
Both sides Hatomepanchi 12mm