Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of P-Test Tube Straight Mouth

P-Test Tube Straight Mouth
Sales Price: 35.99 SGD
Review Rating: 4.22
9 Customer Reviews
5 star 5
4 star 3
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Decorating with marbles
From Japan
On 2017-09-23 22:57:05
The glass was brittle, and four broke. It is a very dangerous thing to have children have.
This review is about item#6664691.
One cycle of fresh flowers
From Japan
On 2017-05-21 17:23:04
I wanted 105 mm, but 100 units are too much to purchase and cut it to 105 mm and use it. I think that it can be used for a hobby if it can purchase about 20 units in all sizes.
This review is about item#6664691.
One burned vase
From Japan
On 2017-03-07 13:31:02
I bought it for single burning. The product is satisfied. However, because there was something that was broken, I made four evaluations. I think that it probably was damaged at the time of delivery. Also, as I needed it in a hurry, I did not apply for replacement.
This review is about item#5783102.
This product is used as a single burner.
From Japan
On 2016-04-22 18:14:47
The quality of the product is very good, thank you.
This review is about item#34846673.
From Japan
On 2016-02-23 16:04:05
It is a good item
This review is about item#05783127.
Used as a sheath tube for underwater lighting
From Japan
On 2015-09-10 11:29:30
I like the size just to insert a 4W fluorescent light, I like it.
This review is about item#34846707.
I use it for one burner.
From Japan
On 2014-06-26 01:53:15
I use it for putting one piece of woodwork. It is just right size for inserting a flower in the field.
This review is about item#06664612.
As a simulated material
From Japan
On 2013-10-14 17:21:59
Although there was prejudice that dimensional accuracy of the pipe would be bad, recently reconfirmed that the size of the glass product is high precision.
This review is about item#06664594.
A substitute for a glass tube with a single burned vase
From Japan
On 2013-07-04 22:20:23
Since it is not the original use of the test tube, it is not easy to write an opinion, but the tube for single-violet disposal is thin and short, so the water runs out soon, so it's not well known. This is very good, as you can ensure enough water.
This review is about item#05783172.
Customer Who Viewed This Item Also Viewed
Cork Stopper
Test Tube, PP
Test Tube Culture
Test Tube
P-Test Tube New Lip
Test Tube Stand Sc Type
Stainless Steel Made Test Tube Vertical
Graduated Plastic Test Tube
Reinforced Rigid Sample Tube R
Test Tube
Test Tube, With A Rim
Test Tube, With No Rim
Test Tube, Rim
Kotobuki oblate bag type
Test tube (made by PFA)
PP test tube
Test tube
A-Test Tube