Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Rubber Stopper

Rubber Stopper
Sales Price: 3.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Stopper of a fish bowl
5
From Japan
On 2017-07-11 16:32:50
It was too hard, moderately soft and very good Because the flower pot was used as a goldfish bowl, the hole was not a perfect circle and it was a little irregular circle, but there was moderate elasticity and just draining the bowl somewhat eliminated the water leak and it was nice
This review is about item#2838132.
Stop the water distribution adjustment port of the pond
5
From Japan
On 2017-05-22 14:40:52
Because the diameter is not straight because of waterproof painting, I was looking for something that can stop water. I tried some before No.34, but No.34 was exactly right. Hardness was reasonable, even if you put in force and pushed in, there was no problem.
This review is about item#2838254.
Used as a stopper for the drain of the hand bowl
5
From Japan
On 2017-02-13 18:46:35
Since the side of the hole to be installed is slightly irregular and leaks water, I use it by rolling the sealing tape for waterworks and using it with a lot of force, but since it is a solid rubber, it can be stopped securely without getting into the hole too much.
This review is about item#2837633.
Used as a cover for low pressure air leakage check of sealed parts
5
From Japan
On 2016-06-07 20:53:53
It is used for sealing of mechanical parts · low pressure air leakage check. Hardness is also good, reasonable so it is good. I used it as a consumable idea, so I tried buying it for durability check, but if there is no problem I will be repeating.
This review is about item#02838071.
Temporary stop of heat exchanger
4
From Japan
On 2016-03-14 14:59:46
There is more than expected effect, I am satisfied. If it dares, if it has a little shrinkage (elasticity) of rubber, could it be able to cope with the change in the inner diameter of steel pipe? However, because the case in this time is a unique place, it was able to correspond with the water stop tape.
This review is about item#02838166.
Sealing
5
From Japan
On 2015-08-04 15:59:08
I think it's good.
This review is about item#02838193.
Used for masking during bead polishing
2
From Japan
On 2014-10-14 16:15:02
When I purchased a rubber stopper of No. 21, the diameter of the dimensional table was only 63, but actually there was only φ 61. The part I bought at the same time was the dimensions as shown in the dimensions. I wish I had made it one larger size.
This review is about item#02838123.
1
Customer Who Viewed This Item Also Viewed
Red Rubber Plug
Silicon Plug
Rubber Stopper
Silicone Plug with Hole
Long Neoprene Stopper
Silicon Plug
Silicon Rubber Plug, Color
Draining Water Cap, No Chain
Plug Viton
Rubber Stopper
Silicone Tube Plugs
Viton plug
Stainless Steel Sieves