Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of NRF Series Circuit Protector

NRF Series Circuit Protector
Sales Price: 12.99 SGD
Review Rating: 4.78
9 Customer Reviews
5 star 8
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Exchange with air compressor circuit protector
5
From Japan
On 2017-11-20 15:00:34
The compressor 's circuit protector which I kept using for about 8 years frequently felt troubled. Although genuine is made in China, the shape and the size and the depth of the mounting hole are completely different, but the thing has also been modified by processing the mounting hole by trial. The result is a complete resurgence! Thank you very much.
This review is about item#34915237.
It is used for electric circuits.
5
From Japan
On 2016-08-15 00:48:10
I am satisfied that I can buy it cheaper than other stores.
This review is about item#06937402.
Used for buffing to give a gloss after floor wax finish
5
From Japan
On 2016-07-24 22:05:51
Machinery which we are hundreds of thousands are also in a state where it is impossible to place orders when they are always purchasing old age, but we were able to replace the circuit protector by virtue of early correspondence and operation became possible. Thank you. Thank you very much.
This review is about item#06937411.
Production safety measures using AC operating equipment
5
From Japan
On 2016-06-30 12:09:56
Fuse BOX Because it is almost the same shape, it was able to be put in a narrow switch box. It is a useful part.
This review is about item#60396594.
Charger
5
From Japan
On 2016-04-15 16:10:00
I have been using it for 3 years to connect the charger and the battery, but it is running without problems.
This review is about item#06937411.
For protection of electric circuits
5
From Japan
On 2015-06-29 21:22:41
I use it in repeat. It is very useful as it does not have to be replaced like a fuse. It is good to extend the scope of application if it is a bit short. Replacement with the fuse holder, the depth may not be able to be taken. I also want to use it from now on because there are many types of capacity.
This review is about item#06937393.
Exchange with existing tube fuse folder
5
From Japan
On 2015-04-15 18:31:14
It is very handy because it is a size that can be exchanged as it is for a pipe fuse folder, and it is very handy because it also eliminates the labor of replacing fuses and inventory.
This review is about item#60395632.
For replacement
3
From Japan
On 2014-04-02 07:24:46
I regret that I thought that the size was the same as before replacement was a bit different
This review is about item#06937402.
Overcurrent protection of control panel electric circuit
5
From Japan
On 2013-04-16 21:47:26
It is easy to use with almost the same size as the fuse holder of the glass tube. It is easy to understand as the button jumps out when triping. It is regrettable that the installation of electric wires is 250 Faston tabs, so if you include the bent part of the wire, you still need some extra depth. Variation of current capacity is large, replacement of fuse is unnecessary and it is convenient so I want to use it in the future.
This review is about item#06937445.
1
Customer Who Viewed This Item Also Viewed
Air Gun
Circuit holder
Circuit Protector CP-A Type
NRLR 1100 series
NRLY 1100 series
Chip 3NU-TPGW-LF
Circuit protector 1115