Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Screw-Type St Type Swivel Caster, Double Bearing, Rubber Wheel

Screw-Type St Type Swivel Caster, Double Bearing, Rubber Wheel
Sales Price: 7.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Truck Piece
2
From Japan
On 2018-03-02 18:51:20
I want you to be able to disassemble with the wheel spindle and screw I feel like lubricating oil because it gives a sound of curing Hard to find
This review is about item#2542757.
For moving the roller conveyor
5
From Japan
On 2016-01-19 16:05:47
It is safe since the width of the wheel is thicker than that of the mass retailer. I think it is durable.
This review is about item#02543082.
Work chair
5
From Japan
On 2016-01-10 01:58:40
I attached it to the monotail iron work frame chair M - TLMS - C (45113284). It became a solid chair.
This review is about item#02543712.
To change the adjuster specification showcase to the caster specification
4
From Japan
On 2015-02-04 13:33:18
It can be used without problems. The mounting bolt part was too long, but it would be good if the length can be chosen.
This review is about item#02543107.
Replacing casters of dolly in use (repair)
5
From Japan
On 2014-09-09 23:30:47
To the carriage with the 75 Ø caster was attached to the one of 100 Φ with this repair as a machine. Absorption of irregularities increased more than expected, it got overcome as much as possible the cracks of asphalt, etc. It was the correct answer by size up. The thing itself is rolling, good direction with good performance with good directional change. In difficulty I ordered things with mounting screws M12, but inch size items arrived. Since I did not have a period to exchange it, I bought a new nut and used it, but I was surprised by a mistake not being monoterous.
This review is about item#02542757.
1