Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Screw Type St Swivel Caster, Double Bearing, W/Stopper, Rubber Wheel

Screw Type St Swivel Caster, Double Bearing, W/Stopper, Rubber Wheel
Sales Price: 8.99 SGD
Review Rating: 4.25
8 Customer Reviews
5 star 6
4 star 0
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Used on a table of a table lathe
5
From Japan
On 2018-05-18 14:56:41
Since the lathes are used within the range of hobbies, the use environment was not so good, so we made a table with casters. Although it moves to the place where sweeping can be done easily when using it, there is feeling that it gets over softly even against the ground with some level difference and it feels good.
This review is about item#2542802.
Mounting under the shelf
5
From Japan
On 2016-01-19 16:00:34
Surprisingly because the width of the wheel is wide, I think that it is hard to wear and it has durability. It is thicker and more secure than those of mass retailers.
This review is about item#02543125.
Mobile device
3
From Japan
On 2015-12-08 09:28:17
Normally no problem
This review is about item#02543274.
Movement of conveyor
5
From Japan
On 2015-10-07 15:18:37
Modified to be able to move the conveyor used in production. It is smooth and can be used without problems.
This review is about item#02542793.
Work platform foot
5
From Japan
On 2015-05-03 19:26:57
Because the workbench itself was heavy, I bought it for moving the workbench, but I was able to move alone, it made it possible to use a narrow space effectively and it was very helpful. Even if the caster is sideways, I think that it is very good because it will turn smoothly when moving.
This review is about item#02543764.
Hobby racing cart conveyor casters
5
From Japan
On 2014-10-07 15:59:44
I am using it as a caster of a hobby's racing cart carrier, but it is very good for running performance. The ordinary hobby of the racing cart carrier caster is φ60 or 75, which is φ100. If the mounting screw is φ100, other companies' products can not be mounted with M16 or M16 equivalent screws, but this can be used with M12 equivalent inch. It is user-friendly enough that you can ask where you bought from a number of other Carter people. The price is equivalent to φ75 and reasonable. I regret that I should purchase it and replace it earlier.
This review is about item#02542793.
As equipment caster
1
From Japan
On 2013-12-03 10:02:08
To screw into the frame, the nut is thin and can not be tightened because the spanner is not hooked. At least, if something is done on the head of the screw it can be shipped with casters that are not tightened, so you can not ship it I replaced it.
This review is about item#02543764.
For dolly
5
From Japan
On 2013-07-08 23:04:03
It is a product with excellent cost performance.
This review is about item#02542793.
1
Customer Who Viewed This Item Also Viewed
SR Threaded Caster
SR Threaded Caster
Swivel Caster, Stopper