Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Metric Thread Sprew for Fine Pitch Thread

Metric Thread Sprew for Fine Pitch Thread
Sales Price: 6.99 SGD
Review Rating: 4.00
5 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Screw repair
1
From Japan
On 2017-11-14 10:34:27
100 pieces of M12-1.25 × 1.0D and M12-1.25 × 1.5D were delivered, It was in a state that 10 sachet sachets were put together in plastic bags each 10 bags each. I understand that packaging is tough, but I'd like you to share things with different sizes.
This review is about item#5495296.
Bolt hole correction for motorcycle
4
From Japan
On 2016-11-12 20:17:57
Especially I do not feel the problem, but there are no objects with a length greater than 2.0D. I purchased this because there is no choice of things with a pitch of 1.25.
This review is about item#5495287.
Screw hole of motorcycle wheel
5
From Japan
On 2016-06-14 12:42:04
It was very satisfying.
This review is about item#05495287.
Bicycle repair
5
From Japan
On 2014-04-30 00:23:43
The rear derailleur mounting screw of the bicycle is specific to M10P1.0, but the screw may be broken due to falling etc. It is a frame exchanging · · ·, if it is a thing with a direct frame attachment, but you can play it if you use this. It is a good idea to insert lubricant slowly while sneaking in? is. However, in the case of aluminum etc., it is better to cut the tap, because it is thin, tongue will break if it is forcibly inserted. Even if the length does not fit, even if it does not have a problem, there is no problem as long as it can be flush and put on the back ledge nippers.
This review is about item#05495235.
Restoration of eye screw
5
From Japan
On 2013-10-14 18:46:08
Care must be taken not to pitch the pitch to insert the sprue.
This review is about item#05495235.
1
Customer Who Viewed This Item Also Viewed
Coil Insert
Sprew P Insertion Tool
Recoil Packet
Recoil Thread Repair Kits
Tools for Remooving The Spruy
Spry S Type Insertion Tool
A Recoil Kit With A Pilot Tap
Tangless Inserts
Inserted Coil Pulling Out Tool
Coil Inserting Tool
Recoil Kit for Spark Plug
SPREW
Supuryu (Bolton packs)
Hand Thread Tap STI-HT
Standard insert (E sart)