Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Portable Case

Portable Case
Sales Price: 13.99 SGD
Review Rating: 4.10
10 Customer Reviews
5 star 6
4 star 1
3 star 1
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Machine maintenance time
2
From Japan
On 2017-10-16 10:08:29
There are two fasteners on the top cover in reverse but normally two people are removed and turned over 180 degrees but inevitably the top cover will be dislocated but at a high place or a place where the scaffold is bad it is not user friendly
This review is about item#6544465.
Voltage measurement, conduction test
5
From Japan
On 2017-02-03 19:27:43
It purchased at the same time with the company analog tester SH - 88TR. As expected it is genuine. I feel that the upper two buttons are sweet when opened, but maybe it's just right if you think you can remove them immediately.
This review is about item#6544465.
To store testers
4
From Japan
On 2017-01-31 18:16:16
I purchased two for analog tester and digital tester. If you use a spacer, I think that an ordinary tester can be stored without play. However, the lid is hook up and down, it seems likely to be lost due to specifications that will come off. The case attached to the insulation resistance meter (PDM 5219S) is a hook that can not come off on one side, it will fit on the back side of the case when turning, so it will not get in the way of measurement and not lose. I think that it is good if there is another idea.
This review is about item#38281941.
Electrical repair
3
From Japan
On 2016-10-03 17:32:33
It is miscellaneous if it is genuine. I only have to think about carrying around. It is hard to put out and the tester bar code protrudes. I think that the partition inside is unnecessary
This review is about item#8748126.
Old type
2
From Japan
On 2015-11-19 07:50:10
I am trying to use it, but Sanwa has not changed since 10 years ago. Because it is used in the field, it is usability too bad! What is different from ten years ago is only a space (partition) to put optional test leads ... · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · · I guess it will be able to sell, even though it is such a fucking shit ...
This review is about item#08748126.
Used for business trip repair.
5
From Japan
On 2015-09-08 15:19:58
It is easy to use and convenient during business trip repair.
This review is about item#08748126.
Electric device inspection
5
From Japan
On 2015-04-21 16:01:44
The building is also cool and the appearance is full of luxury. Moreover, the price is also affordable.
This review is about item#09219113.
Outdoor electrical equipment inspection
5
From Japan
On 2014-06-16 14:29:37
I always use it. It is a very good item.
This review is about item#06790576.
Measurement of electrical work
5
From Japan
On 2013-09-15 22:55:33
Although the lid is designed to be removable, it is better not to come off. I feel inconvenienced to measure by holding the lead wires with both hands. It is difficult to measure the voltage at both ends of a socket of an LED (40 W fluorescent tube type · length 1300 mm) on a stepladder. It is good if you can see the numerical value by hanging on the neck with a long string-like thing and fixing it in front of the chest. Or a long lead wire type (about 1 m) is required.
This review is about item#06544465.
Local work
5
From Japan
On 2013-05-01 17:17:53
I wanted the storage case of Sanwa made CD771 and purchased it. There is an inner pocket to insert the test lead wire when opening the lid of the case, which is convenient.
This review is about item#08748126.
1
Customer Who Viewed This Item Also Viewed
Digital Multi Meter
Digital Multi Meter
Alligator Clip,Clip Adapter
Analog Multitester
Analog Multitester
Analog Multitester
Carrying Case
Portable Case for Hand held I0R Leak Clamp meter
Hard case for Digital Multi Meter 73203
Repairing Holster
Carrying Case
Carrying Case
Red rubber stopper
Carrying Case
Digital Multi Meter
SUTW6 series
Clip Adapter