Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flat Type Soldering Iron, Sheet Metals, K Type

Flat Type Soldering Iron, Sheet Metals, K Type
Sales Price: 66.99 SGD
Review Rating: 3.00
6 Customer Reviews
5 star 0
4 star 3
3 star 1
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
It is used for work such as melting and fixing a part of the molded product of acrylic resin material.
4
From Japan
On 2017-03-21 11:13:18
I am using the thing which melts solder for another purpose, so it is not a selling point of this product, but I think that the point with the switch is a good product from the aspect of safety. It is appreciated as us that there is something more flat in the tip of the trowel.
This review is about item#7291426.
Sheet metal soldering work ...
1
From Japan
On 2017-01-10 17:18:59
It was broken and could not be used for the fourth use after purchase. It was very disappointing. It seems that the wire breakage of the Nichrome heater seems to be bad, and it seems that only the items of this model number are set up for repair parts in the manufacturer site. I felt it was a product without durability in proportion to the amount.
This review is about item#7543085.
Soldering
2
From Japan
On 2016-05-26 16:45:02
I want a size of about 100 W to 150 W. At 200 W the coaters are too big
This review is about item#07291426.
Car sheet metal. Used for filling.
4
From Japan
On 2015-03-04 17:16:06
It was bigger than I expected, so I could be a little smaller. Goods can be used without problems.
This review is about item#07543085.
Automobile sheet metal work
3
From Japan
On 2013-09-04 20:36:18
Separately, I think that there is no particular problem in terms of usability and bad.
This review is about item#07543085.
Pallet restoration work
4
From Japan
On 2013-05-18 22:10:03
Although it is not original use (sheet metal work), it was purchased for use in resin pallet restoration work. Up to now I was working with 100 w of soldering iron, but this is extremely work as 200 w is doubled. Since the soldering tip is flat and solid, it is extremely convenient and satisfying to melt the resin. The disadvantage is again expensive. Expendable parts (soldering tip, heater) are also expensive. I think that those who do not have strength because there is body weight in them do not work for a long time. After that, when the body gets warmer, will the top of the grip rise to a pretty high temperature and will it become quite hot even if you wear gloves?
This review is about item#07291426.
1
Customer Who Viewed This Item Also Viewed
300W Soldering Iron
200W Soldering Iron
Solder Bar
K Type Flat Soldering Iron Trowel
Soldering Iron
Flat Type Soldering Iron, Sheet Metals, L Type
Soldering Iron Junior
HAKKO Junior JI-150W
Soldering Iron SB Type
Flat Type Soldering Iron K and L Replacement Heater
SS Series Type I type replacement heater
Industrial Soldering Iron SM Type
L Type Flat Soldering Iron Trowel