Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Straight type long snap ring plier for holes

Straight type long snap ring plier for holes
Sales Price: 45.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
I plan to remove the hammer drill snap ring made in Germany.
3
From Japan
On 2018-04-06 18:56:32
The pliers hit in a narrow place and it did not reach, solved another jig and settled.
This review is about item#7130392.
Remove address V 125 G driven snap ring
5
From Japan
On 2015-05-19 11:24:15
There is a snap ring at the back of the clutch driven, but it was able to be taken with one shot with KTC pliers. I thought that the diameter of the hole was narrow, but I bought it was the correct answer.
This review is about item#07130392.
Remove motorcycle snap ring
5
From Japan
On 2014-06-01 15:28:44
It is good to make it solid.
This review is about item#07130392.
Bearing exchange
5
From Japan
On 2014-04-29 15:39:39
I used it to exchange bearings with O / H of the brush cutter gear case. The snap ring of the bearing part of the drive shaft was quite deep so it was useful. The tip of the product was thinner than I thought and the strength was a little worried, but it was not a problem, it is recommended.
This review is about item#07130392.
Scooter Driven Pulley
5
From Japan
On 2013-08-20 10:06:07
Long type rarely used, but there was a place that I could not work unless I purchased it. It is SST so long, it has been saved without a shop selling pretty much.
This review is about item#07130392.
1
Customer Who Viewed This Item Also Viewed
Replacement Blade
Snap Ring Pliers, Hole
Bent Long Snap Ring Pliers, Hole
Tip claw set
Bent Long Snap Ring Pliers, Shank
Gasket rear (Y 6)
Long snap ring pliers
Bearings 08130-62047-000