Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Oiles #80 Flange Bush

Oiles #80 Flange Bush
Sales Price: 0.34 SGD
Review Rating: 4.74
43 Customer Reviews
5 star 35
4 star 5
3 star 3
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 20 of 43 Reviews
Homebrew cart direction rudder axis
4
From Japan
On 2017-07-17 14:19:12
It was hard to get used to parts of this hand, but it is a very good slide.
This review is about item#460512.
To the gas gun hammer pivot.
5
From Japan
On 2017-07-06 18:52:50
Used for custom hammer pivot of gas gun. We buy a hammer with a certain ok too because the hole is large so we settle it. It is convenient because it really gathers everything.
This review is about item#460293.
Machine part production
5
From Japan
On 2017-07-02 15:23:07
It is a standard product. It can be used without problems. It is saved because various parts can be bought in bulk.
This review is about item#460415.
Handmade dolly wheel handle Mounted on the moving part of the moving part
5
From Japan
On 2017-05-21 11:00:08
It is a part that is not put in the home center so much and it is very satisfactory to buy it in units of 1 for small quantity use.
This review is about item#460311.
Electric cart steering device
5
From Japan
On 2017-05-15 16:05:56
I thought that there was such a part and purchased it. I am satisfied with enough use.
This review is about item#460512.
During machine maintenance
5
From Japan
On 2017-05-06 16:15:27
It is very helpful because it is a part not sold inside. I will order again.
This review is about item#460801.
Wheelchair repair
4
From Japan
On 2017-04-10 08:19:39
The bush attached to the part where the foot support of the wheelchair is attached was troubled because it collapsed or gone. It was saved because it is perfect for size.
This review is about item#00460485.
Slide work through the linear shaft
4
From Japan
On 2017-04-03 13:47:16
Since the inner diameter of the bush and the shuff and the outer diameter did not match with each other slightly through the linear shaft, there was a backlash so we used a fluorine tape tensioned on the shaft
This review is about item#460257.
To reduce the wear of the slow moving moving part of the prototype and to ensure smooth operation stabilization.
4
From Japan
On 2017-03-09 22:20:01
It is super cheap, it is small as the difference between the inner diameter and the outer diameter is small and it is small, so it was the best for parts of this device.
This review is about item#460275.
Maintenance parts for live steam
5
From Japan
On 2017-02-28 18:14:48
I am thankful for the low price and ease of processing that can handle more than enough of the steam engine's high temperature and humidity!
This review is about item#460311.
Impeller bearing of submersible pump for viewing fish filter wear repair
5
From Japan
On 2017-02-12 18:53:31
I could repair it with a nice touch. I am satisfied with both price and quality.
This review is about item#460241.
Production of simple gearbox
5
From Japan
On 2017-01-13 13:00:07
It is used for a simple gearbox bearing. It rolls accurately and is easy to handle.
This review is about item#460293.
Hinge bearing of lid
5
From Japan
On 2016-12-27 17:46:23
In combination with a brass Φ 4 round bar, it was used for the hinge part of the lid. I used it as a bearing fitted to a thin plate, but the shaft turned smoothly without play.
This review is about item#460302.
bearing
5
From Japan
On 2016-11-04 09:52:43
Because it is thin, it can be designed in a space-saving manner and is useful.
This review is about item#460686.
Used as a polishing machine part
5
From Japan
On 2016-10-14 16:22:49
I have a repeat order. Delivery is also saved soon.
This review is about item#460266.
Robot production
5
From Japan
On 2016-08-17 16:55:16
Because the sliding strength is reasonable as well, if you are not wearing severely you are satisfied because you can use it for a long time
This review is about item#460381.
As a bearing
5
From Japan
On 2016-08-17 10:23:11
It is easy to handle because there is no lubrication, there is no problem with the use feeling.
This review is about item#460406.
As a bearing
5
From Japan
On 2016-06-28 13:22:22
no problem
This review is about item#00460625.
ULP machine elevator horn bushing
5
From Japan
On 2016-06-16 21:36:50
It prevents friction between metals and it is not dirty as it is OIL less
This review is about item#00460424.
Exchange of MIWA lock flange bush
5
From Japan
On 2016-06-07 15:19:09
The bush attached to the lever pin of the face-mounted box lock has worn out and it is detaching.It is a substitute for this because there is no substitute, although some processing is also necessary, it is just right. If you clean up the inside of the box lock and grease up, you can still use it for more than 20 years.
This review is about item#00460905.
1 2 3