Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Point tap (long shank for deep holes) (EX-LT-DH-POT)

Point tap (long shank for deep holes) (EX-LT-DH-POT)
Sales Price: 27.99 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Machine assembly
5
From Japan
On 2017-12-08 18:12:43
It was useful for machining deep parts, using sharpness and strength without problems.
This review is about item#8998123.
Threading of thick steel
5
From Japan
On 2017-01-21 02:14:44
Most long shank taps have a thick shank part, so the maximum thread thickness of about 25 mm is the limit, but for this type it can be threaded to about 50 mm thick. There are few manufacturers making this type of type, so it was very helpful to find them. Sharpness is also good as well as other OSGs.
This review is about item#08998105.
Deep hole drilling at the machining center
5
From Japan
On 2014-09-17 20:49:33
It got well, I was satisfied with durability so so.
This review is about item#08998105.
Deep hole tap stand
3
From Japan
On 2013-07-23 14:44:50
I thought that I wanted to use it for a penetrating tap with a depth of 30 mm and purchased it. Since there was 60 mm under the neck, I felt like to break when used on a machine, so I used it as a hand tap. I thought that I would like more kinds of head length down the neck.
This review is about item#08998105.
1