Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Desk thread saw with speed control

Desk thread saw with speed control
Sales Price: -
Review Rating: 3.00
2 Customer Reviews
5 star 0
4 star 1
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Drawing of toll paint
From Japan
On 2013-02-21 20:00:55
I think that it is easy to process with speed control.
This review is about item#06421475.
Production of wooden toys etc.
From Japan
On 2011-03-07 21:23:33
(1) There is a step of 0.5 mm in the plastic table insert fitted in the part where the yarn saw blade goes up and down and the aluminum table in the surroundings. When the material is moved back and forth, the corner of the edge hits the step, stops, pushes or pulls It will be impossible. Also, the inclination changes with this step difference, or raising the material will cause it to not cut accurately. (2) The accuracy of the plate holding guide, the shaft to be fixed is low, it does not become horizontal, and the fixed position can not be determined accurately. (3) Although the idea of ​​a blower that blows off chips is good, the fixation position precision of the nozzle is poor, and it is not easy to adjust the tip to the chip generation part. (4) It is easy to use when a guide plate for linearly cutting is attached to the plate. Even if there are only a few screw holes in the aluminum table. Well, it would be suitable for the price.
This review is about item#06421475.