Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Color Bit

Color Bit
Sales Price: 5.99 SGD
Review Rating: 4.00
6 Customer Reviews
5 star 4
4 star 0
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
For electrical work
5
From Japan
On 2018-02-16 18:47:24
Precision, mochi, I like it long ago. I think that it is good that it is difficult for the thickness of the bit to become the blind spot to attack the narrow screw
This review is about item#7562021.
Maintenance of the motorcycle
5
From Japan
On 2017-12-25 15:04:43
It was necessary for a long time, otherwise the extent of the decomposition of the exterior of the motorcycle was too big Because it is a round shaft with a hole in part of the exterior, it is enough about 6 mmφ. For a hexagonal axis, the face and face are 6.35 mm, but if it is horny it is about 11.9 mm, you have to make the hole bigger than the foolish hole. Then finished in a hole of 6 mmφ with a lid. Even during the next maintenance, the decomposition range of the exterior, a small merit was born.
This review is about item#48974326.
screw tightening
3
From Japan
On 2017-12-08 10:00:16
It is hard to comment because the picture and the thing I bought are different, but the one I purchased is not easy to lick a tip a bit long, it does not last long, so I do not use the hard tree, but the screw 2.7 mm long and 16 mm long, the cypress I opened the tongue hole 1.8 mm, the cutting edge became round, so it is cheap so it can not be helped, but still about 20 can go.
This review is about item#07561976.
Driver bit
5
From Japan
On 2017-11-23 08:25:31
For ordinary work, I like this bit first, affordable, long lasting strong tip, 3 to 4 mm pilot hole, 150 to 200 screws even with 90 cm screws, the tip can lick if it is 3 to 4 cm screw It is not unbelievable, if it is double-headed screw, it becomes troublesome to replace while confirming which side was when it became one side, so it takes a lot of time, rather than double head screws if there are 50.65.85.100.200 cm each one To have
Vehicle maintenance
1
From Japan
On 2017-09-25 22:47:47
One can not set to the impact driver that scratches licked all around the tip of the hexagon part. You can not use it unless polishing is corrected with a file. Please exchange with good products.
This review is about item#7562021.
Driver bit exchange
5
From Japan
On 2013-09-24 16:38:05
It's a conspicuous color and it's easy to understand with my driver. For now it does not have screw tightening loosening Namel. Is the magnet a bit weak? Well I'm selling parts that strengthen the magnetic force so I do not care too much. It is favorite.
This review is about item#07562021.
1
Customer Who Viewed This Item Also Viewed
Soldering Iron Tip
Color Bit
Color Bit
Colored Bits 10pcs
Colored Bits 2pcs
Ball Point Driver
Ryujin Bit Slim Type
Color bit
V Tamper Proof Torx Bit
Color bit 2 pcs