Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Jet tap

Jet tap
Sales Price: 9.99 SGD
Review Rating: 4.25
12 Customer Reviews
5 star 8
4 star 2
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Attach the chuck to the charging drill and use it.
5
From Japan
On 2017-12-13 17:39:43
This tap is my favorite personally. Even with stainless steel, if you use a tapping spray, you can perform tap work relatively easily, and also have durability and are high points.
This review is about item#6750091.
SPCC t - 1.0 ~ 2.6 Processing of pressed product
5
From Japan
On 2017-11-20 22:17:56
Compared with OSG's EX-POT (general use) ○ Comprehensively durable Stable cutting power until the end of use Pretty sticky even in heavy processing × Low cutting ability (can be said as cutting)? Screw accuracy is somewhat inferior Become In other words, if the optimum pilot hole can be prepared stably and it is a jet tap if it places importance on durability If it is impossible to tap with a pilot hole which is somewhat narrower, or if a beautiful screw is necessary, it can be distinguished from OSG Since 2.6 mm is non-homo so it will fix the notation
This review is about item#6750046.
When screw tapping
5
From Japan
On 2016-05-18 08:41:34
Even if rotation is fast, you tap firmly.
This review is about item#06750091.
Used for remodeling of mold
4
From Japan
On 2014-10-10 13:38:53
It is difficult to understand the difference from other items because it is several pieces at a time but I think that it is lightly cut all the time.
This review is about item#06750177.
Iron crafts, repair, remodeling
2
From Japan
On 2013-09-22 14:20:07
As I mentioned in other size impressions, truly liked the twisted part which breaks when abused if it becomes small to M6, the same size spiral tap (for set screws) using Ishihashi is in use favorite Shallow tip I feel that there is a problem with the screw part I feel like using this size individually, because I feel that the spiral tap is more durable in the through hole than the jet tap for now I purchase this tap (M6) for now If the spiral tap of the same maker is recommended (spiral tap is healthy now so we are planning to purchase it again now is nothing)
This review is about item#06750143.
Iron crafts and repair / remodeling
4
From Japan
On 2013-09-22 14:05:05
Handy to have M6 ~ M10 and describe the impression I have used the M10 is very happy as the No. 1 tap, of price but might be a little expensive to result in a split depreciation many years because it is excellent durability also the same tap useful to the (much satisfaction to design all the way according to the the tap when the fake) M8 you are using yet satisfied, but less frequently used so far (other manufacturers products are not used yet, but the twist part is okay? and since the worry in Ishihashi made favorite) to the M6 ​​decreases as the break and indeed abuse to (spiral tap of the same manufacturers still think personally when the tip of the screw is not perhaps there is room for improvement in the shallow part because not break ) have my selling surprisingly little shops that sell even to go to the city of home improvement (there are more of other manufacturers) since the Mr. MonotaRO leave this If Kere trouble! Dish of "super Recommended" personally and
This review is about item#06750177.
Taps of ss 400 and sus 304
5
From Japan
On 2012-10-03 13:44:10
Sus304 FB-12 * 100 I take a M6 tap 12 mm deep on the 12 mm side (I'm afraid because I am afraid) but I work on other companies' cobalt spiral taps with a considerable establishment. When trying it with a point tap for trial it got a little less settled. When I use this jet tap, I can not break at all, I can get a gang tap. (Since it is a stop hole, it is necessary to discharge the trim part along the way), we changed all our taps (except M30) to the product of Ishihashi Seiko. By the way, it seems that Oino is nicknamed better than Tenohii than red.
This review is about item#06750091.
Screw stand of iron · SUS
5
From Japan
On 2012-01-22 01:01:21
Very good. The cut is also good, durability is outstanding. So it is hard to break. I would recommend it to everyone.
This review is about item#06750064.
Tap for stainless steel material
5
From Japan
On 2009-10-11 17:42:23
Since it is Ishihashi Seiko (manufacturer product) it is not complaining.
This review is about item#06750143.
Tap working of mild steel
5
From Japan
On 2009-06-15 22:43:23
Good break, tap work fast
This review is about item#06750091.
SS400 steel tap working plate thickness 19 mm, etc., SUS plate
5
From Japan
On 2008-08-29 20:23:46
You can tap work at ease
This review is about item#06750091.
SS400 steel tap working thick plate
1
From Japan
On 2008-07-07 22:14:59
Even with a thick plate of 20 mm, tap work can be done easily without increasing the diameter of the prepared hole
This review is about item#06750177.
1
Customer Who Viewed This Item Also Viewed
Cobalt Jet Tap
Spiral tap
New tap metric thread screws
Stainless Jet Tap
GEKKOU Drill Blister Pack
Tafuretto - L
Jet tap
  • Jet tap
  • ISHIHASHI SEIKO
  • 12.99 SGD
Cobalt Spiral Tap
Jet tap
  • Jet tap
  • ISHIHASHI SEIKO
  • 15.99 SGD
Jet tap
  • Jet tap
  • ISHIHASHI SEIKO
  • 14.99 SGD