Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Radial bristle Marguerite disk With 50.8 mm (2 inches) of outside-diameter axis of 6 mm

Radial bristle Marguerite disk With 50.8 mm (2 inches) of outside-diameter axis of 6 mm
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Grinding work of rust of aluminum, stain, iron etc.
5
From Japan
On 2017-12-14 16:13:03
Easy to get to the tip and corner of the abrasive, so efficiency of polishing work is improved.
This review is about item#7167702.
Metal, polished, polished
5
From Japan
On 2016-06-17 11:51:20
Previously, I was using for ruther, so I tried using it for drilling, I am satisfied, I want to arrange other numbers as well
This review is about item#07167736.
It is used for honing inside the cylinder of a brake caliper of a motorcycle or a car.
5
From Japan
On 2015-02-21 04:12:02
I am awfully saved when cleaning the seal groove when disassembling the disc brake. Especially for the old caliper aluminum caliper, the effect is perfect. I did not think that this product could be bought at Monotaro at a single point. I am using No. 120, which is adjusted by the number of revolutions of the rider. I hope this thing with small width and diameter. After that, there is no saying if this item gets a little more major and the unit price goes down.
This review is about item#07167702.
It is used for work that does not want to cause scratches and wear on the metal such as rubber-like gasket removal of machine parts.
5
From Japan
On 2013-02-26 02:54:30
The brush part has good abrasion resistance and can be used for a long time without axial shake. Many uses are also useful, such as metal rust removal, gasket peeling, painting undercoat treatment and many other uses. I would appreciate it if the price is a little cheaper, but it may be a reasonable price from the usable life.
This review is about item#07167693.
1
Customer Who Viewed This Item Also Viewed
Radial Bristle Disc
Radial Bristle Brush
Throttle Valve
Spiral wheel
Fiber Wheel Brush
Radial bristle disc