Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pillow Block Unit Ukp Type

Pillow Block Unit Ukp Type
Sales Price: 19.99 SGD
Review Rating: 4.50
6 Customer Reviews
5 star 4
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
When maintenance of air conditioner
5
From Japan
On 2016-11-07 22:14:50
Thank you for dealing with the next day delivery on the same day despite ordering on Sunday. It is a weekend to use, but there is also a meeting etc etc and it will be helpful!
This review is about item#7196156.
Agricultural machines
5
From Japan
On 2016-09-07 21:56:56
it's the best. I would like to use it from this as well.
This review is about item#7196131.
Securing the shaft
5
From Japan
On 2016-02-15 18:09:14
The price was cheap and could be used without problems.
This review is about item#07196156.
Tractor repair
3
From Japan
On 2015-12-28 15:06:35
Even if there is a comment with the separately sold as if it is easier to buy if it is in an adapter bundled type.
This review is about item#07196165.
Tire bearing
5
From Japan
On 2015-08-18 11:19:51
I designed it as a bearing of a homemade towing car, but it feels very good. I am satisfied.
This review is about item#07196165.
Repair of customer equipment
4
From Japan
On 2013-06-02 21:44:36
Adapters should also be combined together. Why, I do not know the meaning if the adapter is sold separately. Make a mistake because you put the adapter on the photo.
This review is about item#07196156.
1
Customer Who Viewed This Item Also Viewed
Pillow Block Unit Ucp Type
Pillow Blocks
Bearing Adapter H300X H2300X
STB IS pulley IS-B3
Pillow Block Unit UCP-C Type
UKP pillow-shaped (tapered bore)
JIS V pulley C-1
Pillow type unit taper hole type