Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Snt Ultra-Thin Spanner

Snt Ultra-Thin Spanner
Sales Price: 4.99 SGD
Review Rating: 3.91
11 Customer Reviews
5 star 4
4 star 4
3 star 2
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
It was used to tighten the nut in the narrow gap between the crank case and the cylinder.
4
From Japan
On 2018-02-26 17:28:26
I managed to fasten the nut somehow, but I think I could work more easily if it was a little longer.
This review is about item#2193563.
Wheelchair Maintenance
3
From Japan
On 2017-11-24 15:22:22
I bought it because it is a necessary tool to remove a caster (front wheel) of a wheelchair, The thickness of 4 mm was just barely available and could not be used depending on the car model. Since the old rubber-tightened casters have become hard, The spanner side also needs some strength and it is difficult to choose a tool.
This review is about item#2193572.
Motorcycle Maintenance
5
From Japan
On 2017-08-15 12:49:20
Though it is thin, the strength is sufficient. It is useful for adjusting mirror and clutch wire.
This review is about item#2193536.
Maintenance
3
From Japan
On 2017-07-14 21:25:00
I purchased it because I needed a thin spanner. The amount is also cheap, and it can be used without problems.
This review is about item#2193563.
For wheelchair maintenance
4
From Japan
On 2017-06-14 19:16:52
I purchased it for permanent use as a wheelchair maintenance. Usability is a future task
This review is about item#2193572.
Maintenance of construction machinery, agricultural machinery, etc.
5
From Japan
On 2017-04-24 07:59:05
If you are using a low nut such as an accelerator wire or a rod in double, you can not access it unless it is this item. Although it is written as if there is a problem in strength in the review of the other person, it is impossible to give out strength with this thickness even if there is tool steel used, I think that it is necessary to devise and use it. I can not repair with force.
This review is about item#02193545.
For motorcycle maintenance
4
From Japan
On 2015-07-30 13:33:00
I bought it as a substitute for an inch tool. I think COSPA is a high product. It is handy because it can not be accessed because it is thick as it is a normal tool.
This review is about item#02193554.
Exchange casters
1
From Japan
On 2015-07-22 09:41:42
Used for exchanging casters. Although it was c53c high carbon steel indication it lost to the bolt and the spanner was able to scratch the dent itself. I feel too much. Is it really C53C class? When we measure with calipers, is not it that the spanner's caliber 19 mm is too large (19.75 x 19.5 mm taper) to cut too much? It looks like a Chinese product that can not be put to practical use only by shape.
This review is about item#02193572.
Rutter tip exchange
5
From Japan
On 2014-05-17 14:26:03
Accuracy is good It does not understand durability because it does not apply much torque so it is good
This review is about item#02193536.
For bike adjustment
4
From Japan
On 2013-11-19 20:21:50
It was as thin as expected. Work is easy.
This review is about item#02193545.
Exchange chair casters Other
5
From Japan
On 2013-06-07 07:16:24
Use it for parts that are not wide and that do not fit in.
This review is about item#02193536.
1
Customer Who Viewed This Item Also Viewed
extremely thin  spanner set
Ultra Thin Spanner
Double-ended spanner
9x10.0mm Thin Wrench
Spanner (standard type/mm size)
Flat Wrench Set
Double-ended spanner
Liner Spanner
Sn Double-Ended Spanner
Hammer Caster Fitting Wrench
Thin opening spanner
Mounting Plate Spanner
Thin Wrench Set
Combination Spanner
Smc Micro Double-Ended Spanner