Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hexagon-head axis CL hole cutter (cobalt bimetal)

Hexagon-head axis CL hole cutter (cobalt bimetal)
Sales Price: 25.99 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Used to gouge one pipe to weld a round pipe to a round pipe when making a handrail
5
From Japan
On 2016-12-02 14:44:22
I always use Tamami Industry Holson, but it's easier to use than the things like. There are things I think if the height is a little longer.
This review is about item#7589951.
Electrical construction
5
From Japan
On 2016-01-23 15:11:25
Used with 18 V drill driver. It is a cheap and excellent hole saw that can withstand use by professionals.
This review is about item#07589811.
work
5
From Japan
On 2015-11-04 18:56:34
Is good
This review is about item#07589976.
Weak electric wiring work
5
From Japan
On 2013-06-10 14:39:31
It is used for drilling for wiring at the site, although it opens a hole to the iron plate of several millimeters thick from the gypsum board, it can be used without particular problem.
This review is about item#07589933.
To drill through the wire
5
From Japan
On 2013-02-15 12:47:02
It is mainly to drill a hole in the board, but a hole often opens even if there is a tree. I still do not know how much the cutting edge will be consumed.
This review is about item#07589906.
1
Customer Who Viewed This Item Also Viewed
Bimetal hole saw
Impact hole saw
Bimetal Cutter
HSS Hole Saw
FCL Hole Cutter
Bimetal Hole Saw J Shaped
Cordless hole saw
Impact Hole Saw