Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of FRP drill

FRP drill
Sales Price: 26.99 SGD
Review Rating: 4.89
9 Customer Reviews
5 star 8
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
In order to install the LED working light on the outside of the FRP camper, I purchased it for drilling for installation and trying to make a hole to pass the cord.
5
From Japan
On 2018-03-31 21:00:49
The cutting edge was attached so that the cutting edge of the drill would follow the circumference, and as the blade was rotated, it cut through the circumference, dust did not scatter and it was possible to drill a hole smoothly. I was impressed. It is excellent. As expected it is for FRP.
This review is about item#7587036.
FRP product drilling
5
From Japan
On 2017-06-29 10:07:06
7.5 mm has been discontinued and very troubled. . . If it is 7 mm to drive a 5 mm ebina nut, it will not come in unless it is to be scraped off with a little reamer It was drilling at 7.5 mm. As I got 7.5 mm, I was thinking about making it new When we saw the site we stopped handling · · ·. I would like you to resell by all means. Thank you.
This review is about item#7587072.
Drilling processing of FRP thick plate
5
From Japan
On 2017-06-21 07:50:53
FRP 30 mm thick plate started to be cleanly cleaned, the position was not shifted with a cemented carbide 3-core structure, the exit was also cleanly cut, and the time and labor for finish processing became unnecessary. Even so, since FRP is a glass material, unreasonable drilling processing shortens the life of the drill bit, and we can not agree with impossible pressing work. It is a product you want to cherish.
This review is about item#07587221.
Drilling in FRP products
5
From Japan
On 2016-12-20 19:53:32
The 6 mm thick FRP plate gel coat was sputtered and the hole opened without chipping. Because of the Brad Point, the center position does not shift.
This review is about item#7587045.
Drilling of FRP
4
From Japan
On 2016-05-08 18:59:53
If there is a lineup of 5 mm or less ...
For processing of FRP products
5
From Japan
On 2016-02-08 14:48:24
I will have a beautiful hole. I like it very much.
This review is about item#07587045.
Drilling of FRP
5
From Japan
On 2015-04-05 17:11:06
Bali can also be drilled cleanly without permanent purchase. If the price is a little cheaper ... 5 mm more will be saved
This review is about item#07587063.
Mainly for drilling of materials for fishery
5
From Japan
On 2012-08-05 06:17:09
Holes are very smooth! Improvement point, とき when ri became worse, ___ ___ ___ 0 ___ ___ 0
This review is about item#07587307.
Make a hole in a resin octopus used in fishery
5
From Japan
On 2012-05-16 17:46:01
I was surprised by the sharpness beyond expectation. I was able to make a hole very comfortably, but I will price the price very much. I want follow-ups on how to sharpen after it gets worse.
This review is about item#07587307.
1
Customer Who Viewed This Item Also Viewed
FRP Hole Cutter
Handy bag (Standard)
Air Orbital Sander
Core drill for FRP (set)
Sand wheel
Carbide cutter straight shank drill
Core drill for FRP (cutter)
FRP for the center drill