Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Screw Type 420A Swivel Caster, Nylon Wheel Urethane Volume Wheel

Screw Type 420A Swivel Caster, Nylon Wheel Urethane Volume Wheel
Sales Price: 2.99 SGD
Review Rating: 4.67
6 Customer Reviews
5 star 5
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Glass showcase
From Japan
On 2017-10-03 21:03:42
I attached it to the legs of a glass case that is heavy and difficult to move. w 3/8 was also studied. I can move it.
This review is about item#8009224.
For rack
From Japan
On 2016-05-23 16:17:48
What comes with the assembly rack with a bonus, if the load is applied, the turning of the caster becomes very bad. This product is very smooth because it uses bearings in the swivel portion. If the wheel is made of rubber, it will deform in the long term. The urethane winding is used comfortably without deformation or vibration.
This review is about item#08009267.
It is for the table of the special tool at the work site
From Japan
On 2015-10-29 17:49:15
Next time I will make the wheel bigger.
This review is about item#08009242.
Office chair casters
From Japan
On 2014-12-15 08:45:04
It was possible to install without any problems.
This review is about item#08009267.
Put it under the chair for moving.
From Japan
On 2014-04-01 02:27:58
It is comfortable and can be used forever without rubberity than rubber cars.
This review is about item#08009215.
Chair repair
From Japan
On 2013-03-19 13:50:15
Part of the caster chair used at the store was damaged, and it was replaced and repaired by oneself. Quality is "excellent". I asked for a spanner at the time of replacement, but my misunderstanding did not match the thickness and purchased a very thin spanner of 4 mm thickness from another company. If you need additional casters, I'd like to request it here by all means.
This review is about item#08009267.