Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Nut Breaker

Nut Breaker
Sales Price: -
Review Rating: 3.00
6 Customer Reviews
5 star 1
4 star 1
3 star 2
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Destruction of rusty nuts
4
From Japan
On 2012-12-01 15:19:52
Necessary, the nuts are 13 mm and 17 mm across flats, but as small as possible is as good as possible, it is up to 16 mm, but other manufacturers also made this product. I thought it would be nice if there were for 13 mm to 17 mm if possible.
This review is about item#08250934.
Demolition work
3
From Japan
On 2011-12-19 20:49:47
I was able to break it without problems though the nut was cracked or suspicious. Just break the hexagon nut fastening the breaker immediately. It became difficult to use when the tip turns round. Currently I use it with holding by hand.
This review is about item#08250943.
Removal work of mini car muffler
5
From Japan
On 2011-12-04 18:44:45
I was able to destroy pleasantly rusted nuts.
This review is about item#08250934.
To remove the nut under the car body, replaced by the result burner grill.
1
From Japan
On 2011-05-14 08:50:21
I can not use it although I do not know whether it is not suitable for use.
This review is about item#08250934.
Destruction of rusted nut
2
From Japan
On 2011-04-26 02:06:19
I thought that it was convenient to break the old vinyl house but purchased, but the plates with nuts were all bent inwards and could not be used. If the ring is thin 2 millimeters or so, it may have been a comfortable work
This review is about item#08250943.
When forcibly removing the rust thread of the demolition article
3
From Japan
On 2007-12-11 13:51:04
I am replacing the breaker itself because it breaks.
1
Customer Who Viewed This Item Also Viewed
Nut Splitter
Nut Breaker
Nut Breaker
Nut Cracker
Nut Breaker
4pcs Nut Splitters
[10-27mm] nut splitter
[12-16mm] nut breaker
22-27mm Nut Breaker
[16-22mm] nut breaker