Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Urethane Re-Coil Air-Hose

Urethane Re-Coil Air-Hose
Sales Price: 27.99 SGD
Review Rating: 3.20
5 Customer Reviews
5 star 1
4 star 1
3 star 1
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Various work
3
From Japan
On 2017-05-18 21:19:56
Inner diameter 5 π is a bit thin. I saw everyone's review and bought 8 m, but it's actually 6 m. If the curl is too tight, and trying to extend it further, the repulsive power of the return is too strong, it is hard to hold, rather than working.
This review is about item#8377537.
Motorcycle maintenance
2
From Japan
On 2017-03-31 17:11:38
Due to its compact size, the resistance seems to be large, and the long hose will surely reduce the air volume of the air gun.
This review is about item#8377546.
Adjustment of tire air pressure such as tractor light truck farm equipment
2
From Japan
On 2016-09-30 20:42:44
I purchased comp racers for the first time, I could not understand the terms of the fittings, I thought that the joints were unified, I was in trouble. The tank capacity now is a little bigger and the application expands. The full tone of air pressure is very fast, but the sound is high
This review is about item#8377537.
Air tools for car maintenance
4
From Japan
On 2016-08-10 18:45:22
As the product image, the coil part is gathered compactly (diameter is also 5 to 6 cm) so it does not take up a place to get tangled. On the other hand, I think that it is practical range up to 70% of product length because there is resistance to stretch. ※ If you stretch your eyes a lot, you will be pulled so far.
This review is about item#8377546.
As an air hose
5
From Japan
On 2015-06-25 22:03:33
It is very good because it is not possible and it is inexpensive and low price.
This review is about item#08377546.
1
Customer Who Viewed This Item Also Viewed
Air Coil Hose
Spiral Air Hose Yellow Line Series
Spiral Zero One
Coil Hose
Spring Urethane Coil Hose
Spiral Air Hose
Screw Air Hose
Urethane Re-Coil Air-Hose
High power coil hose
High-Power Re-Coil Hose
Urethane Coil Hose 2.4m
Strong Coil Hose
Coiled Air Hose