Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Bolton Pack Crimping Nut, Light HeadAluminum

Bolton Pack Crimping Nut, Light HeadAluminum
Sales Price: 11.99 SGD
Review Rating: 4.29
7 Customer Reviews
5 star 4
4 star 1
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
During motorcycle maintenance
4
From Japan
On 2016-08-09 11:45:55
I used it for stopping the cowl of the scooter. I purchased it cheaper than the home center.
This review is about item#8340297.
Production site
5
From Japan
On 2015-10-13 21:37:56
Working with this product became easier, I would like to use it again. I think there is a short one that can be used in places without depth.
This review is about item#08340236.
I use it as a mounting bracket of a roof type spoiler · wing.
3
From Japan
On 2015-05-02 00:59:55
On the thin head shape of the material M5, the buckling does not become uniform, and it is easy for some to bulge on the thin head surface. If it is M6 it is not a problem but because the buckling strength is high, hand nutter is painful if there is no large size
I am using it for thin iron plate etc. when attaching to aluminum plate.
3
From Japan
On 2014-07-30 00:27:22
There is a time when 4 M slips slippery with force adjustment, so I wonder if there should be some more guts. I am using 5M with a nice feeling without problems.
This review is about item#08340324.
The key points of the bike ...
5
From Japan
On 2014-04-13 20:30:32
Complaints with price and strength! True TRUST ★
This review is about item#08340281.
Nut caulking to aluminum chassis
5
From Japan
On 2013-08-05 13:25:10
I made caulking jigs and used it, but the buckling strength was so high that the screws were sometimes pulled out. I am desperate by nut tightening at the moment. It is more convenient to have a model with weak buckling strength.
This review is about item#08340324.
It was used instead of tap for aluminum chassis (t1.6).
5
From Japan
On 2013-08-05 13:21:04
I am using it for case processing of amp which I am producing as a hobby. I pulled out the jaw of the rivetter and created the caulking jig. It is more convenient to have a model with a weaker buckling strength.
This review is about item#08340297.
1