Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Crimped Nut, Steel, Flat Head

Crimped Nut, Steel, Flat Head
Sales Price: 11.99 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Car interior processing
5
From Japan
On 2015-11-19 11:09:23
The home center had only made of aluminum and was looking for steel. If made of steel it is good that the threads are not easily damaged.
This review is about item#08339904.
Car product installation
5
From Japan
On 2014-08-14 23:30:09
Because it is used for the body steel plate of a car, I used a steel crimp nut in consideration of potential difference. If it is a rivet it will be permanent installation, but crimp nut will be removable. In order to caulk, the special tool "Nutter" is necessary.
This review is about item#08340017.
I am using it for assembly
5
From Japan
On 2013-12-13 16:36:39
It is saved as it can be used without reinforcement of the back plate.
This review is about item#08339895.
Used for mounting the cowl stay of the TZR50R racer
5
From Japan
On 2011-06-16 15:49:50
I used it to bolt the cowl stay to the main stay of the square pipe, but when I used it, I really have to use a proper nutter, but if it is an aluminum blind nut that I installed with pulling it with a bolt I thought that it was easy but I bought it iron, it was pretty tough but I could install it without problems Because it is not used so much, it will be saved if you can sell it in 2 units or fewer number
This review is about item#08339904.
1
Customer Who Viewed This Item Also Viewed
Pop Nuts
  • Pop Nuts
  • NIPPON POP RIVETS AND FASTENERS
  • 4.99 SGD
  • 4.666670(3)
LOBSTER Hand Nutter
Rivet Nut
Aluminum Flat Head Nut Packed