Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Blind Rivets Stainless Steel,Packed Product

Blind Rivets Stainless Steel,Packed Product
Sales Price: 15.99 SGD
Review Rating: 4.00
8 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Maintenance of the boat
5
From Japan
On 2017-09-08 20:25:45
The number is small and easy to purchase The price is attractive The goods are relieved
This review is about item#8340613.
Maintenance of yachts
5
From Japan
On 2017-06-16 16:56:06
I used aluminum rivets, but I can be used for parts where strength is needed, so I am pleased to get it at a low price. I would like to place an order if it will be lost in the future.
This review is about item#08340604.
Own fishing tool
5
From Japan
On 2016-12-14 16:16:03
Because it is stainless steel it was the best and easy to use for the sea.
This review is about item#8340753.
During machine maintenance
5
From Japan
On 2016-07-22 22:48:36
It is handy because it is strong and reliable to install and convenient
This review is about item#08340893.
For bike silencer repair
4
From Japan
On 2016-04-06 09:17:28
It is a review about 4.8φ / d = 3.2 to 4.8. It was the cheapest item in All SUS, so I tried using what I thought, but there is no problem at all. · The shaft has a slip groove. · The thickness of the brim portion seems to be slightly thinner compared to 4.8φ of other products. · I worked with a two handed hand riveter, but there was no problem with one. · I tried it even with a one handed riveter but it was hard and gave up.
This review is about item#08340622.
Rivet work
2
From Japan
On 2016-03-30 16:51:33
I used the muffler to replace the glass wool but I chose the rivet according to the pilot hole but when I shake the muffler after the work, something Kachakacha sounds! Is it? It seems to be firmly fixed, but something uneasy. It seems that not all sounds are coming from rivets. Do I need special tips? Please tell me. Even though it was a sturdy sturdy because it is a part with vibration. I worked with rivettes compatible with stainless steel rivets, and since a lot of it is not necessary, subsidy is saved, but I want a division of the highest ranked rivets. Since monotalou is convenient, I want it to correspond.
This review is about item#08340622.
Assembling aluminum products
1
From Japan
On 2015-05-25 20:25:47
Since the shaft is not firmly fixed to the flange, when the shaft is downwardly used, the shaft falls into the product, and both the product and the rivet become unusable. There was not such thing in the rivets of other companies that we used to date. I wish I had purchased first-class maker goods!
This review is about item#08340622.
FRP repair
5
From Japan
On 2014-09-05 16:48:59
If the finish after riveting is more beautiful if it is more beautiful, in normal use there is no problem at all. It will be saved because it does not break up on the way like cheap rivets.
This review is about item#08340604.
1
Customer Who Viewed This Item Also Viewed
Standard rivets (stainless steel and stainless steel)
Standard rivets (aluminium / aluminum)
Blind Rivets, All Steel
Blind Rivets, Stainless Steel
Sten blind rivet
Engineering grasping EG
Blind Rivet
Blind Rivet