Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Mountain Shaped Tool Box

Mountain Shaped Tool Box
Sales Price: 24.99 SGD
Review Rating: 4.46
13 Customer Reviews
5 star 8
4 star 3
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 13 of 13 Reviews
As a tool box for easy working
5
From Japan
On 2017-07-07 16:18:53
I got lost as far as Monotaro original, but I chose this one that looks good. It is exactly good with the amount of tool to put and size. Because it is a simple operation, I use this tool when I do not need a lot of tools. I also have solid construction of the handle part.
toolbox
3
From Japan
On 2016-06-09 16:59:49
It is a general tool box.
This review is about item#33432147.
toolbox
4
From Japan
On 2015-10-19 16:13:49
Although the size notation was done, it is super delicious when you see the real thing! It might be a little hesitant if you look at the shop front? I still do not use it so much, but welding the handle to the size? I am concerned.
This review is about item#08379987.
Storage of car maintenance tools
5
From Japan
On 2015-04-14 20:38:02
It is saved to be able to store long ones. A lot of tools enter.
This review is about item#33432147.
Tool holder
5
From Japan
On 2014-10-22 18:14:39
Even if you decorate it is cool. Working, the tension rises.
This review is about item#08380023.
Tooling of electrical work
5
From Japan
On 2014-07-24 13:24:06
I bought it for a protection box of a long torque wrench, but its length is good, but I also want you to build shallow depths
This review is about item#08379987.
In a case for a disk grinder ...
5
From Japan
On 2014-04-12 11:23:43
I bought it for storage of Makita's disk grinder 9533B. Some cases for disk grinders are made of plastic, but they made it metal, probably because they could crash by hitting them. I could store the AC cable without stress too much, so I thought it was somewhat larger, but this size was good.
This review is about item#37311084.
12.7 torque wrench, spinner handle, requires a tool box to accommodate, purchase
5
From Japan
On 2014-03-09 18:34:10
The spinner handle 450 mm, the length of the torque wrench, 456 mm, I want a tool box that fits it, purchasing Y-455 B, the point of purchase was described that the length was 459 mm with internal dimensions. Arrived and put it in, it fits pitally. In addition, I use a set of 12.7 square ratchet wrench, socket, extension bar, joint etc. The box is also strong and can be used with confidence. Since it is used while putting in and taking out from the door, size is exactly good size. I think that if you have a tray with a tray, you will be more convenient.
This review is about item#08380075.
Machine maintenance
5
From Japan
On 2014-02-03 18:16:58
Very easy to use, capacity was exactly right.
This review is about item#37311084.
Factory maintenance tool box
4
From Japan
On 2014-01-31 10:58:25
It can store various tools collectively, and is easy to use. However, it is better if there is storage space for haberdasheries (bolts, nuts, screws, nails, etc.).
This review is about item#08380075.
Tool storage
5
From Japan
On 2012-06-19 21:17:10
It is pretty good. Rather considering the price, it is done very well. It is a very different from the original tool box of \ 980 which I bought at some other tool shop. The tool box of a certain store only folds a thin iron plate, and the end part is sticky or pointy, but this is molded by pressing, so it is smooth, without seams, folds. The price difference is 2 to 300 yen, but the satisfaction level is completely different. This time we chose a red box like a tool box, but there seems to be some differences in color and shapes, so I'd like to buy silver per turn with appropriate reasons.
This review is about item#08380023.
Tidy
3
From Japan
On 2011-08-19 09:54:01
no problem!
This review is about item#08380023.
4S
4
From Japan
On 2011-02-21 09:58:17
It's okay!
This review is about item#08380023.
1
Customer Who Viewed This Item Also Viewed
Tool Box
Two-Stage Tool Box
RS Dream Box
Suitcase Tool Box
Trunk Tool Box
Suitcase Tool Box, Tray
T-Box
Hip Roof Tool Box Silver
N Type Double Door Box
Tool Box
Medium dish tray
Y Type Box
Suitcase Tool Box
Toolbox Inner Mat
Mountain-type tool box
Trunk Tool Box
Index hook (hook)