Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Double-Sided Eyelet Made Of Aluminum

Double-Sided Eyelet Made Of Aluminum
Sales Price: 3.99 SGD
Review Rating: 4.00
14 Customer Reviews
5 star 8
4 star 1
3 star 3
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 14 of 14 Reviews
Sheet eyelet processing etc.
3
From Japan
On 2018-04-23 20:19:10
I hope you can purchase it a little more cheaply. Because it uses a small amount, it will take years to consume. . .
This review is about item#8339651.
Reinforcement of sheets of vinyl house
1
From Japan
On 2018-03-13 21:37:34
I could not use it because the dimensions did not match (it did not fit with the caulking tool)
This review is about item#8339633.
Adding eyelet of track sheet
5
From Japan
On 2018-03-02 17:15:17
Simultaneously ordering because there were few eyelets on the double-sided eyelet punch set. I was able to work without worrying about failure.
This review is about item#8339651.
To the seat eyelet
3
From Japan
On 2017-05-19 14:52:52
Purchased along with the punch for the seat eyelet, it can not be tested because it fits a little punch and it is a holding item.
This review is about item#37295483.
To a camper
5
From Japan
On 2017-04-17 07:20:43
Used on the roof of the bank bed to fix the flexible panel.
This review is about item#08339633.
Leather product strap hole
2
From Japan
On 2017-03-03 19:00:50
As a function of the product, although it is the specification of hope reason, because the excitement around the shape of the female side is misaligned, it does not finish cleanly, the good one is about 10%. Since the price may go up, I want you to make it a product with high precision.
This review is about item#39449733.
Sheet
5
From Japan
On 2016-08-17 20:06:07
It was easy to handle when stopping it because it is aluminum.
This review is about item#8339642.
Add a sheet eyelet
3
From Japan
On 2015-10-23 21:03:42
Because it seemed that the ball of the eyelet that matched with the eyelet punch (for inner diameter of 7 mm) used so far was going to be lost, when I bought P - THP - A 7 with an inner diameter of 7 mm, the actual inner diameter of the delivered item was 6.2 mm, I understood that the numerical value mentioned was nominal size, I ordered a returned P - THP - A 8 large size 1 large. P - THP - A8 matched the desired item with an actual inner diameter of about 7.4 mm. We were able to correspond quickly from returning to reordering and shipping, and finished purchasing with satisfactory results. Thank you for adding the description of the actual size inside diameter to the explanation of this kind of product on this occasion. Aluminum eyelets are just good in hardness, easy to use, strong against rust, so I would like to use different sizes.
This review is about item#39449751.
Nylon cord self-made
5
From Japan
On 2015-04-16 11:40:18
Because replacement nylon cord of mowing is expensive, I bought it for making my own. It is common to buy things of this kind at the home center, but if you have no time to go free shipping, I think that it is good to purchase it and pick it all at once. Since the catalog is described in detail, it is convenient to order most of the things at home if you do not have any trouble.
This review is about item#39449733.
Used to fix the seat
4
From Japan
On 2015-04-13 09:19:03
Surprisingly, aluminum tends to be deformed. As I got used to it, the loss was reduced.
This review is about item#08339667.
Repair of eyelet with 30 kg of rice bag
5
From Japan
On 2014-12-21 14:05:44
I could repair missing eyelets. I am glad that the eyelets are restored.
This review is about item#08339667.
It is very helpful to use it for the pop of plastic cardboard etc.
5
From Japan
On 2014-06-27 19:22:18
I used it to prevent a hole from being torn by a cable wire.
This review is about item#08339624.
For reinforcement of mounting hole of display plate
5
From Japan
On 2014-04-10 13:27:42
I am happy that you can sell roses.
This review is about item#08339642.
Car interior, exterior equipment production
5
From Japan
On 2013-04-24 13:18:55
This product needs caulking tool, but it was able to do the crimping thoroughly even with the caulking comma alone.
This review is about item#39449751.
1