Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pole

Pole
Sales Price: 4.99 SGD
Review Rating: 4.73
11 Customer Reviews
5 star 8
4 star 3
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Used to investigate deposition thickness of unstable earth and sand during field investigation of civil engineering design
5
From Japan
On 2017-01-14 11:45:58
It is a satisfactory product in terms of size, strength and price as it is less than 1 meter in most sites and no problem. However, there are times when it is necessary to measure more than 1 m in rare cases, so I think if there is a product of a size up a notch, specifically 1.3 m in length and 9 mm in diameter.
This review is about item#8289407.
As a target for practicing the car
4
From Japan
On 2016-05-25 00:33:38
Used as targets for parallel parking practice. There is no problem because it is cheap and stands out to some extent and is strong.
This review is about item#08289407.
Photograph shooting etc. on field survey
5
From Japan
On 2016-05-02 09:27:58
Anyway, the price is cheap, I think that it is good to disposable, but tomorrow tomorrow, painting is also beautiful, the picture taking is also good, it is unnecessary to throw away.
This review is about item#08289407.
Survey etc.
5
From Japan
On 2014-12-03 16:38:29
It is cheap and rich in size so it will be saved
Used for forest survey
5
From Japan
On 2014-10-03 15:18:43
The part of the stone is also good. It is very good.
This review is about item#08289407.
Photo
5
From Japan
On 2014-08-04 20:01:37
There is also paint thickness and it is firm. It can be used quite well until it can not be rusted. The photos are well taken.
This review is about item#08289434.
Positioning in the skill test
4
From Japan
On 2014-06-16 22:22:21
I think that it is difficult to fix the water yarn by painting the surface, so if you have painted it or you have slip it on the pole itself.
This review is about item#08289416.
Used on the border of the neighbor
5
From Japan
On 2014-06-03 18:29:27
It is easy to pierce into the soil and the upper part is in a circle, so it is easy to use through the rope, I think that the paint is firm so I think it is strong against rust, I like it because price is cheap.
This review is about item#08289407.
Civil engineering work
5
From Japan
On 2013-06-05 14:02:01
Although it is a standard item, it is not easy to use, but it is good because it is cheap.
This review is about item#08289416.
pin
5
From Japan
On 2013-04-26 13:07:29
Quality is everywhere the same. The price is cheap, 30% bought, there is no loss.
This review is about item#08289416.
Building site
4
From Japan
On 2013-03-01 13:24:02
It is OK with moderate size. Explicit points are easy to understand when leaving in the photo record.
This review is about item#08289434.
1
Customer Who Viewed This Item Also Viewed
Pole, Red and White
Aluminum Photo Rod
High Pole
Survey Pole
Aluminum Rod Light
Pin Pole
  • Pin Pole
  • YAMAYO MEASURING TOOLS
  • 4.99 SGD
Newal Rod
Ribbon Rod Both Side 60E-2
Pin pole steel
Tora bar Pin Pole steel
Point Base Konoe Double
Pole
Pin Pole
Wooden Pole
Survey Pole
Pin Pole
Pole Tora bar Pin
Pin Pole Stand
Precision Pin Pole