Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of WA grinding wheel (No. 1)

WA grinding wheel (No. 1)
Sales Price: 14.99 SGD
Review Rating: 4.25
12 Customer Reviews
5 star 6
4 star 3
3 star 3
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Welding finishing processing
5
From Japan
On 2018-02-08 20:43:14
I am just satisfied with just good hardness, 255 sizes.
This review is about item#8433941.
chamfer
4
From Japan
On 2017-07-26 16:21:15
Actually I wanted about # 100, but since this is the only one I bought.
This review is about item#8434045.
Chamfering and deburring of steel
5
From Japan
On 2016-04-02 16:37:59
no problem.
This review is about item#08433826.
Rough cutting
3
From Japan
On 2015-11-28 16:46:44
It is good.
This review is about item#08433975.
Rough correction of the missing saw blade etc.
3
From Japan
On 2015-07-22 19:29:12
We use it to correct the missing blade such as a circular saw by scraping the tip a little like a taper. Compared to other manufacturer's grinding wheels, when cutting saw blades a little, it is slightly decreasing, but since there is no problem with grinding, it is planned to purchase continuously. I would like to purchase if there are things that are thinner and harder (outer size 255 mm, thickness 9.5 mm - 10 mm, degree of connection N) if you have nothing particular about the grindstones.
This review is about item#08433941.
Tool polishing
4
From Japan
On 2015-05-16 17:23:06
I did not know that until purchase it was made by Crayonton's overseas factory. At the work site, I also gave an opinion that the outer diameter becomes smaller than the previous ones and it becomes impossible to use immediately if I dress it. However, I am satisfied that the use feeling of the product itself is good and I do not complain from the site. If possible, we would appreciate it if you can also make products with the same outside diameter as before.
This review is about item#05366734.
Used in a grinder
5
From Japan
On 2015-03-09 09:36:25
Since it is a maker item, it was possible to use it without purchase problem.
This review is about item#08433826.
Polishing operation
5
From Japan
On 2014-05-02 19:09:12
I hope that it is a monotaro brand, more cheap.
This review is about item#08433871.
Using a circular part to polish the spring
5
From Japan
On 2014-01-30 18:04:16
I hoped for peelable glue the other day. The area of ​​the paste was very small for the orders this time. Did it correspond quickly? Thank you very much.
This review is about item#08433975.
It is used to polish the spring using the circular part.
4
From Japan
On 2013-12-10 10:21:43
In order to use a wide surface, I remove the label, but it is difficult to peel off, so I'd like to change it to a glue that can be easily peeled off.
This review is about item#08433975.
When you make a drill with a tooth missing or a tip of a scribe bar
5
From Japan
On 2011-11-14 12:19:57
The feeling I used is smooth, and the teeth of a thin drill of about 4 mm can also be cleaned beautifully. We mainly use 3.2 mm - 16 mm drills, but we are satisfied as we can make all drill teeth with this grindstone.
This review is about item#08433871.
Brushes of leather shoes (polishing for bottoming)
3
From Japan
On 2008-07-24 20:37:07
It's hard not too hard, it's just good for polishing the skin. Since the adjustment ring of the mounting shaft is not attached, it was necessary to machine the shaft.
This review is about item#08433792.
1
Customer Who Viewed This Item Also Viewed
GC grinding stone (No. 1)
Wa Whetstone, White
Grinding Wheel
A grinding wheel (No. 1)
SG Wheels
Magnifier
Flat-shaped grinding wheel 85A
Flat-shaped grinding wheel DA
Flat-shaped grinding wheel 32A