Customer Reviews of Illuminated Selector Switch Ar22 Series
|
Sales Price: 15.99 SGD
Review Rating:
![]() 5 Customer Reviews
|
|
---|
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
It is used as a power supply switch for the equipment.

From Japan
On 2018-01-05 11:16:29
It also uses the power on display. It is inexpensive and easy to use.
This review is about item#8509216.
Switchboard switch Purchase of replacement items due to breakage.

From Japan
On 2016-08-17 16:35:37
The product itself is satisfactory enough. I evaluated it as dissatisfied. I think that it is not a thing that can clearly understand to anyone the content notation such as the product specification etc. It makes a dissatisfaction evaluation. Although the actual item is with lighting in particular, although we are using 30 V LED, there is no indication that there is no indication that there is a separate power supply unit. (Transformer only notation) Despite the fact that there is also a product with a transformer, I have not made that notation, it is really regrettable.
This review is about item#8509225.
Preliminary when factory machine parts fail

From Japan
On 2016-08-15 19:16:20
I am grateful if the price is cheaper a little more
This review is about item#8509225.
control panel

From Japan
On 2014-12-18 18:12:57
As a changeover switch, it was able to be used satisfactorily satisfactorily without problems.
This review is about item#08509216.
Control panel production

From Japan
On 2014-03-10 18:40:25
It is the same as usual because it is used many times and it is easy to use
This review is about item#08509216.
1
Customers Who Viewed This Item Also Bought
<<
>>
Separate type roller follower NAST ZZR (Shield type , With inner ring , Spherical outer ring)
NIPPON THOMPSON (IKO)
30.99 - 82.99 SGD