Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Selector Switch AH165 Series

Selector Switch AH165 Series
Sales Price: 22.99 SGD
Review Rating: 5.00
1 Customer Reviews
5 star 1
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
Stereoscopic parking device (repair of operation panel)
5
From Japan
On 2009-08-20 15:21:12
I appreciate the model that has not changed for many years. It's a structure that allows the knob (key cylinder) side and the contact side to be detached, but it seems to be the reason why the nail of the detachable part breaks each time it breaks. Since it can be used on the control panel of the parking lot for substantially 7 to 8 years, it can be said that it was sufficiently consumed, but I felt that I could use more if this nail did not become easy to disengage. This time I bought the knob type, but in the case of the key it will come off at the nail part if the pushing force is strong. In the case of a knob type, even if the pushing force is strong, it will not come off, but when detaching the panel intentionally, such as detaching the panel during maintenance, the claws seem to weaken. So, I think that it is better to use without detaching as much as possible.
This review is about item#08508062.
1