Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of NJC series JIS standard medium type metal connector straight plug

NJC series JIS standard medium type metal connector straight plug
Sales Price: 7.99 SGD
Review Rating: 3.54
13 Customer Reviews
5 star 4
4 star 3
3 star 3
2 star 2
1 star 1
The reviews are automatic translation.
Showing 1 - 13 of 13 Reviews
When creating control cable
4
From Japan
On 2017-06-01 15:05:15
I hope to have a smaller size to fit the cable
This review is about item#8556615.
For equipment connection
2
From Japan
On 2017-04-05 20:43:53
I bought it because it is a seven star, but the accuracy of the screw is bad and the feeling when tightening is bad. It is big difference with NJW system.
This review is about item#8556581.
Between the controller box and sensors and actuators
1
From Japan
On 2017-03-16 17:45:11
It is a standard product. I use it very often and I can see it in Achirakkira. But did you perform a sensory test to sell it? I would like to ask the seller. Bad screwiness of the first screw, gaze feeling which you feel all the while you are turning. Well, attaching and detaching the connector is instantaneous, so it does not matter. I hope it can be used for the time being, but I will not adopt it as a device to put in my hand. People inside the manufacturer, do not get angry often? Oh, the solder riding is very common.
This review is about item#8557236.
LED connection
5
From Japan
On 2016-03-11 15:12:53
It is the second purchase.
This review is about item#08557175.
Connecting the power cord
3
From Japan
On 2016-02-29 15:22:38
It is on the price.
This review is about item#08556667.
Less choices in 15 A class
4
From Japan
On 2015-03-21 16:38:05
There is no option to choose 4 pin 15 amperes as much as possible and I always use this but I do not need to use it even outdoors, so if there is something smaller for indoor use and say no shape etc. Negative elements that need to choose a combination also If you choose one male or female, if there is a link on the partner side to be fitted, there are many combinations with male · female · positive · reverse as users as it is linked I think that it is too hard to paste, but I want you to work hard (since there are also many points, so if you mistake it by any chance, since the claim is attached, I think that there is a risk) The good of this series is that the contact rotates, The point that it is easy to solder Other people, I have a comment that lead wires should be soldered but I want to attach the harness I want to use directly, so absolutely with lead It is a pair
This review is about item#08556676.
For relay between control unit power supply unit and control board.
3
From Japan
On 2014-07-17 14:52:26
We ordered a 12-core plug and receptacle with a shell size of 20, but the delivery date was about 5 days off. Because I used it in pairs, I thought it was okay to have it match with the late ones with the delivery date. I see the real thing, I think that it is a bit difficult for soldering because pin spacing is too narrow for the presbyopic progressive, so I will try to repurchase the large NCS series metal connector again. (It would be nice if the catalog shows dimensions that show pin spacing etc.)
This review is about item#08556633.
The old connector became well, so I tried to replace it and purchased it
4
From Japan
On 2014-07-13 18:08:01
Since the solder raising work has not done so much recently, if I could have done a bit of hard work, I felt this work was comfortable with the solder worked lead wires, it ended.
This review is about item#08556615.
For controller production
2
From Japan
On 2014-06-11 14:23:14
Although it is a product used for many years, I want you to make it lighter and more compact while having specification compatibility
This review is about item#08557166.
To tractor wiring
3
From Japan
On 2014-01-23 02:32:44
I regret buying a female female who does not fit this time. I thought that it might have been done without making a mistake if it was sold as a set.
This review is about item#08556572.
Used for prototype
5
From Japan
On 2013-09-13 21:42:28
Use it as a condition where it does not cause poor contact at the power connection part.
This review is about item#08556597.
Used for the power connector of the audio amplifier.
5
From Japan
On 2013-01-18 12:24:39
The current capacity is larger than the cannon connector, and it is made of aluminum die-casting and has a high-class feeling.
This review is about item#08556545.
Motor cable
5
From Japan
On 2011-08-15 14:49:54
Although it is making NC milling machine, it is easy to solder the thick eye line with cable wiring. Since the pin soldered part rotates (idling), you can easily bring the soldering iron without twisting the cable side. A little, but the ease of working is Pikaichi. The price is also cheap, so it is affordable as it is solid.
This review is about item#08556581.
1
Customer Who Viewed This Item Also Viewed
Panel to Cable Wire Relay Connector SRCN Series, Straight Plug
Panel to Cable Wire Relay Connector SRCN Series, Panel Mounting Receptacle
NET series metal connector straight plug