Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Electromagnetic Switches And Contactors, Th-N Type

Electromagnetic Switches And Contactors, Th-N Type
Sales Price: 61.99 SGD
Review Rating: 4.82
11 Customer Reviews
5 star 10
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Improvement of wiring
5
From Japan
On 2015-10-09 17:43:53
To be able to explain the contents of the product more.
This review is about item#08583836.
Replacement due to equipment failure in automatic board
5
From Japan
On 2015-08-11 11:21:08
The position of the screw hole for relay mounting did not match, but we have installed it as new and used without problems.
This review is about item#09254253.
Motor protection
5
From Japan
On 2015-07-09 23:24:34
It can be used without problems by changing from other manufacturers.
This review is about item#09254253.
hydraulic
5
From Japan
On 2015-03-28 09:35:37
There is no problem exchanging from Yaskawa Electric made.
This review is about item#09254244.
Protection of 3 phase motor
5
From Japan
On 2015-01-31 17:07:25
I was in trouble because I do not understand the combination well
This review is about item#47839145.
Repair of control panel
5
From Japan
On 2014-03-22 20:44:18
The correspondence was quick, the item arrived quickly. The breakdown of the electric parts is a lot of time and it is very helpful.
This review is about item#08583766.
Since the motor was changed from 0.1 kw to 0.2 kw, the thermal relay was changed to the proper one.
5
From Japan
On 2014-01-17 13:19:41
Since the motor was changed from 0.1 kw to 0.2 kw, the thermal relay was changed to the proper one. As it was instant delivery, I was able to replace it immediately. Especially used without problems.
This review is about item#08583723.
Electrical protection of machinery
3
From Japan
On 2013-05-20 22:13:15
It was cheaper than the dealer's purchase and the delivery was quick.
This review is about item#08583793.
Since rust appeared in the magnet switch, it was exchanged at the same time when it was exchanged.
5
From Japan
On 2013-03-27 11:11:14
1, because there was no content that became a problem because I ordered by looking at the same manufacturer + model number as the replacement item to be replaced. 2, Since there was a big difference between fixed price and purchase price, there was also anxiety, but it is a familiar domestic manufacturer item and purchased. 3, It is useful for procuring because there are no electric materials and water supply members nearby.
This review is about item#08583696.
I used it as a set with an electromagnetic contactor for an air compressor.
5
From Japan
On 2012-08-30 13:02:18
Mitsubishi Electric's open type electromagnetic switch (order code 08582533) that I purchased this time was published as a representative image with Thermal Relay this time. However, the answer to the inquiry was an e-mail with "Thermal relay optional". Therefore, as a result of ordering separately, things of the posted photo were sent and I was allowed to return only the relay. Regardless of the accuracy and completeness of the product we are pleased to be able to use it without any problems, but I would like to ask a reliable answer about product knowledge. Regarding other countermeasures, it is quick, reliable and hard to beat.
This review is about item#08583793.
The motor which I used so far became smaller, and the thermal relay was changed from 18 A to 15 A.
5
From Japan
On 2012-06-04 12:35:55
It is more costly to change only the thermal relay than to replace the entire electromagnetic switch. Since the thermal relays of various settings exist in the frame of MSO - N20, I often use it.
This review is about item#08583836.
1
Customer Who Viewed This Item Also Viewed
Thermal Relay Standard Form Type
Thermal Relay Standard Form Type
Thermal relay MS-T series