Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Flat Cable Connector, Types In GeneralXg4 Box Type Plug

Flat Cable Connector, Types In GeneralXg4 Box Type Plug
Sales Price: 1.99 SGD
Review Rating: 4.33
3 Customer Reviews
5 star 2
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
RC model connector board
3
From Japan
On 2018-05-14 16:29:33
Easy to use but insufficient pin strength. When inserting / removing several times, one pin broke.
This review is about item#8593286.
To install IDE connector of favorite personal computer
5
From Japan
On 2015-10-08 10:38:31
Fujitsu slim tower desktop machine ESPRIMO FMV-D 5290 is favorite. There are two SATA connectors (Port 0 and Port 1) on the menboard, and the SSD and the HDD are connected. I installed a DVD multi-drive, but the 40-pin through hole for IDE was filled with solder and the connector was not mounted. It is owned by the same model, sucking the solder of the through hole and attaching the IDE connector, it becomes possible to use the IDE connected DVD drive. With reference to the article, we also implemented the IDE connector and saw it. The BOX type 40 pin IDE connector generally differs from the pin header which is not in circulation as it collects information with the net which can not be obtained at medium. Confirming that Omron's XG 4 is conforming, as MonotaRO also sold it, soon I ordered and installed it. After installing the IDE connector, the BIOS also recognized the DVD drive and it was worth remodeling.
This review is about item#08593356.
Board connector
5
From Japan
On 2015-02-17 19:06:06
Thank you for always responding quickly.
This review is about item#08593322.
1