Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Terminal-Block Xw4 for Printed Circuit Boards

Terminal-Block Xw4 for Printed Circuit Boards
Sales Price: 1.01 SGD
Review Rating: 5.00
4 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews .
Used as part on board
5
From Japan
On 2016-05-19 15:57:47
It was used as a part on the board. I am using it without problems.
This review is about item#08595011.
For external connection from printed circuit board
5
From Japan
On 2016-02-22 00:34:16
I bought it for making test power supply using general purpose printed circuit board. The same kind of terminal board was using Akihabara which can be purchased at almost half price, but it is a difficult point that it is necessary to process the hole. However, it is good to be able to mount it on a general-purpose printed circuit board as it is. I can also use it when raising the substrate, so I made a library. In the future this will be the basis.
This review is about item#08595072.
As a terminal block of the control interface board
5
From Japan
On 2016-01-17 16:01:13
I think that it is equivalent to MKDSN 1, 5 / 3-5, 08 of Phoenix Contact Company. As a 5.08 mm pitch product, it is short and the height of the board can be suppressed, but the maximum diameter of the wire is slightly smaller, so you need to pay attention when inserting more than one. It was extremely cheap and saved, for selling bulk. Although I bought a number at once, it is slightly minus that it takes time to open it as it is individually wrapped.
This review is about item#08595072.
I use a lot from the printed circuit board to input and output
5
From Japan
On 2015-05-18 18:55:47
It is convenient because you can secure the pitch even when concatenated. Although I did not care much at first at first, I think that fixing the wiring is more reliable than similar products, I think that other things will not be used in the future.
This review is about item#08595072.
1