Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Motor Breaker

Motor Breaker
Sales Price: 42.99 SGD
Review Rating: 4.86
21 Customer Reviews
5 star 19
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 20 of 21 Reviews
Machine maintenance
5
From Japan
On 2017-03-01 14:38:14
I could exchange work without problems. I will continue to buy it with a monotalrow.
This review is about item#8581684.
Control of agricultural house
5
From Japan
On 2016-11-29 21:31:08
I will use more than 20 in a few years, but there is no problem. I am handy because it is handy and affordable.
This review is about item#8581675.
For protection of three-phase commercial ventilation fan
5
From Japan
On 2016-10-22 20:47:10
Both cost and function are satisfied. Nothing to say.
This review is about item#8581666.
Breaker replacement
3
From Japan
On 2016-08-25 21:27:27
As a replacement reserve, it is saved
This review is about item#8581702.
3 horsepower motor control
5
From Japan
On 2016-03-26 00:59:06
It is useful because it is an agreement type and easy to use and shipping is also fast.
This review is about item#08581711.
Dryer
5
From Japan
On 2016-01-08 09:04:18
It was used for dryer, it worked without magnet and condenser.
This review is about item#08581727.
Replace due to breakdown
5
From Japan
On 2015-09-17 08:58:13
Because it is a domestic manufacturer, it can be trusted.
This review is about item#08581693.
As a breaker for the drain pump
5
From Japan
On 2014-08-03 15:48:01
It was easy to install even in a small and narrow place.
This review is about item#08581675.
Ventilator breaker
5
From Japan
On 2014-07-04 12:09:56
Easy to purchase at low price, product is no problem.
This review is about item#08581657.
Mainly to the motors of woodworking machinery
5
From Japan
On 2014-05-20 15:07:03
Satisfactory improvement point small in feeling of use None in particular
This review is about item#08581727.
apparatus
5
From Japan
On 2014-04-10 09:33:42
It is saved because the delivery date and price can be checked quickly.
This review is about item#08581675.
Connection of processing machine
5
From Japan
On 2014-01-21 18:07:17
I can use it without problems.
This review is about item#08581702.
To the power line to the motor
5
From Japan
On 2013-08-07 12:50:23
It was better to be cheaper than other stores and mail-order sites. The correspondence was also like mono tallow and it was quick and likable.
This review is about item#08581727.
Wiring work
5
From Japan
On 2013-04-28 19:18:41
There was no problem.
This review is about item#08581675.
Air compressor switchgear
5
From Japan
On 2013-03-20 19:16:04
Attaching a motor breaker, use it once. There was nothing to worry about.
This review is about item#08581702.
I used it for repairing the machine.
5
From Japan
On 2013-02-01 22:07:38
It was saved because the arrival of goods arrived early. Unlike the previous part, it was necessary to process the hole unlike the previous part, but the dimensions were also known smoothly in the catalog, so it was able to be done smoothly. The operation was able to be used normally without problems. Thank you very much.
This review is about item#08581675.
For business
5
From Japan
On 2012-09-21 22:10:07
It was easy to use and easy to install.
This review is about item#08581657.
Rice paddy harvesting machine to prevent burning the motor at times
4
From Japan
On 2012-09-17 12:29:53
Because it is a breaker, it will be this
This review is about item#08581666.
Three-phase motor installation required for safety
5
From Japan
On 2012-09-14 09:35:41
Because it is a leading manufacturer product, it is safe and secure There is nothing wrong
This review is about item#08581684.
By powering up the motor
5
From Japan
On 2012-08-10 19:10:00
It is more efficient due to miniaturization.
This review is about item#08581702.
1 2