Customer Reviews of 2Flute DLC Mill
|
|
---|
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Milling machine, machining center processing

From Japan
On 2017-07-29 16:57:11
We processed the A7075 material with reference to the cutting conditions posted on the maker's website, but as a result we were able to perform satisfactory processing. I think that it will be necessary in the future to confirm the durability, but we are satisfied at the present time.
This review is about item#8644395.
Cutting of pure aluminum (A 1070 P) panel

From Japan
On 2017-06-19 16:24:01
It was used for cutting 2.5 mm of pure aluminum (A 1070 P) panel. Because it was a thickness not sold at A5052, pure aluminum was too thick, so I did not want to cut it, but I could cut it without difficulty.
3mm The grooving of the end mill was cut by a total length of 5m, but the coating was in a clean state without peeling off.
It is very cost effective. I will try to align each thickness
This review is about item#8644255.
Small parts processing

From Japan
On 2017-06-08 10:00:40
Even in the case where the workpiece support can not be firmly formed, I realize that there are fewer burrs and vibration and fewer breaks. I am happy that the cutting surface is beautiful.
This review is about item#8644492.
Aluminum jig manufacture and others

From Japan
On 2017-04-04 15:37:06
If it is a duralumin series it may be naturally possible to cut lightly, but welding seems to be small even with a sticky pure aluminum, I think that it is best if it is for aluminum. I feel a little kiriko of groove cutting whether the strong twist is successful.
This review is about item#8644492.
Dry cutting aluminum plate

From Japan
On 2015-12-22 14:39:41
You can crack crunchy with dry cut. The price is about twice as much as the aluminum only mill of non DLC coat, but it is the best balance as it is half compared with other DLC coated products of other companies.
This review is about item#08644255.
T company aluminum panel panel processing

From Japan
On 2014-12-10 13:10:12
I used an aluminum mill without a coat, but it did not work well, but when I used cutting oil I got better a little ... but using this mill is amazing! The work crisply broke and the work was serious.
This review is about item#08644255.
1
Customers Who Viewed This Item Also Bought
<<
>>
1AL End mill for aluminum
Mitsubishi Hitachi Tool Engineering (former Hitachi Tool Engineering)
27.99 - 37.99 SGD