Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Nose drill 13 type (1/2)

Nose drill 13 type (1/2)
Sales Price: 48.99 SGD
Review Rating: 4.71
7 Customer Reviews
5 star 6
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Used for workpieces
5
From Japan
On 2018-04-02 09:20:30
This size is not in the home center, but when I go to the machine shop to go buy it is somewhat disliked by eye line from the top so I can buy it here and it will be saved. But I came to the delay.
This review is about item#8667163.
Drilling into plastics
5
From Japan
On 2017-09-14 18:13:27
Quality, price and satisfaction, especially ordered in the morning and delivered the next morning and was in time for work. Thank you.
This review is about item#8667197.
Drilling of test jigs
3
From Japan
On 2016-05-01 15:45:21
Drilling of a polyacetal round bar, biting occurs because of the additional processing of 10 mm to 18.5 mm in the prepared hole, and further additional hole processing is required.
This review is about item#08667066.
Drilling
5
From Japan
On 2015-12-23 17:03:39
I always use it sharpness.
This review is about item#08667197.
Drilling into thick steel sheet.
5
From Japan
On 2015-05-06 23:51:55
Sharpness is wonderful only for natirrill. V Grooving ensures that the chuck does not slip and reliably rotates. However, something was not written on the attached plastic part, there is no description in the maker catalog on the net, and the plastic protection ring is attached for preventing the shock at the time of penetration in the document of the other explanatory note. Finally I understood the content. I just threw it away unless I noticed it. If there is an explanation somewhere, it will be better.
This review is about item#08666971.
Drilling in cast iron
5
From Japan
On 2015-04-05 13:24:45
I tried drilling in the drainage bowl of the casting of the bridge, as expected it was able to be dawn up to the end of all the nosdoryl 16 points. The price is expensive, but it is worth it.
This review is about item#08667093.
Drilling
5
From Japan
On 2012-06-12 19:31:36
There are also missing items for ordering 12, 6, 1, delivery is 12, 10, 9, There is no talk at such a delivery date, can not somehow be managed.
This review is about item#08666996.
1
Customer Who Viewed This Item Also Viewed
Cobalt Drill Bit
Straight Drill
Noss dril type 6 (1/4)
Cobalt Drill Bit
Drill Bit
Drill Bit
Triangular drill (10 type)
Triangular drill (13 type)
Drill Bit
Noss Drill 10 Type
Shingo Shinko Shaft 6.5 Drill
Noss drill (HSS)
Drill Bit 13mm