Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of HSS Straight Shank Drills

HSS Straight Shank Drills
Sales Price: 3.99 SGD
Review Rating: 4.26
58 Customer Reviews
5 star 35
4 star 10
3 star 9
2 star 1
1 star 3
The reviews are automatic translation.
Showing 1 - 20 of 58 Reviews
Maintenance
5
From Japan
On 2017-11-20 09:30:17
Tooth wear is also less, inexpensive and very useful. It is a good product.
This review is about item#8731441.
Tool stock
5
From Japan
On 2017-09-16 16:52:26
Although I bought it for the first time, the price was affordable, it was easy to use.
This review is about item#8731362.
When pilot hole is opened at the time of making wood deck
4
From Japan
On 2017-04-20 15:38:03
Although I have not used it yet, strength seems to be no problem, I am looking forward to use.
This review is about item#8731371.
Cospara is good
5
From Japan
On 2017-04-17 07:56:15
I want a long hole because of the test hole, but I purchased it because it is quite expensive if it is a DYI shop.
This review is about item#08731554.
When pilot hole is opened at the time of making wood deck
5
From Japan
On 2017-03-23 15:18:24
I am satisfied that I can open it without losing the hardness of hardwood.
This review is about item#8731326.
Drilling into sheet metal
5
From Japan
On 2016-08-04 09:39:52
I am well off, so I would like to continue using it in the future.
This review is about item#08731457.
During machine maintenance
5
From Japan
On 2016-06-08 16:31:31
I am saved by cost reduction.
This review is about item#08731387.
Metal Processing
3
From Japan
On 2016-05-31 14:48:55
Especially not possible nor impossible
This review is about item#08731317.
Drilling
1
From Japan
On 2016-05-26 17:10:24
Used to drill 2 mm into a 1.6 mm thick steel plate. Both of the two, when we drilled about 8 holes, it is refreshing around the middle. The package is a letter of MADE IN KOREA.
This review is about item#08731301.
Drilling
5
From Japan
On 2016-03-25 17:37:27
Good!
This review is about item#08731371.
Koukann
5
From Japan
On 2016-03-09 21:00:44
Iiyo
This review is about item#08731301.
Drilling of stainless steel plate
5
From Japan
On 2015-11-23 07:13:14
It gave a bit of digging and cutting, and no positioning punch was necessary at all.
This review is about item#08731301.
Drilling
5
From Japan
On 2015-11-19 21:59:17
I drill 4, 5 mm without punch, but it is very handy.
This review is about item#08731405.
Drill a hole.
5
From Japan
On 2015-09-22 00:45:03
For the control panel made of steel plate, hole formation was made. It is a good drill that makes it easy to put out the center. I just wanted to evaluate it properly after I did it because I have not punctured the "little harder" steel.
This review is about item#08731475.
work
5
From Japan
On 2015-09-08 05:51:27
I am very happy because it is not available in neighboring stores.
This review is about item#08731484.
Automobile
5
From Japan
On 2015-08-18 15:08:59
I am satisfied with the low price I used for opening holes for wiring.
This review is about item#08731301.
Drill a hole in the iron
3
From Japan
On 2015-05-10 15:17:41
It can be used normally.
This review is about item#08731484.
Drilling in wood
3
From Japan
On 2014-10-28 18:17:17
Durability may be subtle.
This review is about item#08731362.
I drilled a hole in order to attach a clamp to the steel bar.
5
From Japan
On 2014-10-22 13:28:08
It was easy to use and was well off.
This review is about item#08731405.
Automobile processing improvement etc.
5
From Japan
On 2014-09-10 23:40:19
Today, I received all 6 types of goods. Many drill blades I had used until now have gotten bad, so they bought a cheap item (3 to 10 mm) in bulk. I would like to purchase repeat if sharpness is good. Because high blade also break easily, I would like to pay attention to how to use the drill and I would like to try another type of product if the sharpness is bad.
This review is about item#08731335.
1 2 3