Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Carbide Rotary Bur

Carbide Rotary Bur
Sales Price: -
Review Rating: 4.40
5 Customer Reviews
5 star 2
4 star 3
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Deburring
4
From Japan
On 2017-03-24 16:55:14
Although I think it is very good for deburring, I hope it is more durable, but at first it is better to disconnect, but if you use it for a while it will be bad
This review is about item#8743077.
Stainless steel
4
From Japan
On 2014-08-18 10:31:25
Please also describe what kind of steel you can use. For now, I am satisfied and using it.
This review is about item#08743077.
Chamfer of iron, SUS, metal
5
From Japan
On 2014-06-27 12:19:00
It is installed on the air grinder and used. I can cut it well, but I think that the eyes are pretty rough, so I need it for finishing. I will confirm the durability from now. I hope the price goes down a bit.
This review is about item#08743086.
Chamfer in a narrow place
5
From Japan
On 2011-12-27 14:02:05
The blade length is short and easy to use.
This review is about item#08743077.
Although it is mainly stainless steel processing, I use it to make a long hole after opening a drill hole.
4
From Japan
On 2011-02-27 22:33:33
Although there are not many problems when used normally, I think that it is the same as not being able to use because the eye is too fine as it becomes a tip because it becomes a taper against the tip of the blade. Even at the tip, if it is more coarse eyes it is difficult to get clogged up to the tip and I think that 100% of the cutlery can be used.
This review is about item#08743086.
1
Customer Who Viewed This Item Also Viewed
Master Carbide Bur C
Master Carbide Bur A
Master Carbide Bur C
Master Carbide Bur A
Master Carbide Bur C