Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Dark Color Waste Cloth (Black)

Dark Color Waste Cloth (Black)
Sales Price: 19.99 SGD
Review Rating: 3.09
11 Customer Reviews
5 star 2
4 star 4
3 star 0
2 star 3
1 star 2
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Dirty wiping
5
From Japan
On 2016-09-29 16:41:13
The amount was also cheap, the work efficiency was good.
This review is about item#8745816.
Disposable, for cleaning
4
From Japan
On 2016-02-16 09:36:34
I bought it for cleaning outdoor and water field, but the purpose has been reached. The price is cheap, so cost performance is outstanding. It is easy to organize and it is a good impression that it is contained in bags by 1 kg each.
This review is about item#08745807.
Waste oil treatment
5
From Japan
On 2015-07-16 15:10:24
Used in waste oil treatment. Goods are sufficient in contrast to prices. However, I want you to remove a small edge that can not be used anyhow.
This review is about item#08745816.
Dirt wiping
4
From Japan
On 2015-01-16 00:22:57
I think that it will be easy to use if the material is made constant a little more. I think that it is a sufficiently bargain product because the price is cheap.
This review is about item#08745807.
Tool cleaning, sealing material, paint wiping etc.
4
From Japan
On 2014-09-18 12:00:06
I used a lot of cotton but I did not need anything high, so I made it.
This review is about item#08745816.
Machine maintenance
2
From Japan
On 2014-01-21 13:10:25
G It is hard to use because the bread dough enters.
This review is about item#08745816.
Wiping OIL work
1
From Japan
On 2012-05-21 19:18:05
Although it does not want much as it is inexpensive goods, there are things like strips in sizes too much, it is just like a piece of cutout and usability is bad. Although it says that absorption is bad on the product publication page, it was a comment for oil work, but I do not smoke too much. I do not mind color patterns etc, but the material is too bad Many things that can not be sucked are many Many things that do not serve as waste Well 5 KG is the only thing that can be used is at most 2 to 3 KG place? Is not it a way of adsorbing it, is it also good for polishing what does not care about metal or scratches, so that the cloth is hard so that it can be laid for dirt prevention? I would like to expect sizes that are not bandlike at the same time as future quality improvement.
This review is about item#08745807.
Wiping off oils
2
From Japan
On 2012-02-28 14:03:04
I bought it because I was aware that bad absorbency is bad, but complaints came from the scene on the bad weather. It seems that it was impossible to wipe off any oil at all with the damp cloth. In a different department I turned it for work to wipe off the heavy oil containing the metal roughly. Even if it does not become beautiful, it seems to be okay if it works like wiping heavy oil spilled on the floor for the time being. Because equivalent absorbency is not good, I think that it is better to purchase it after considering the use purpose well at the time of purchase
This review is about item#08745807.
I am using it to wipe off the oil of the mold and machine.
4
From Japan
On 2011-10-04 09:00:47
Anyway it's cheap! I threw it away, so I looked for cheap ones. Hygroscopicity is inferior to knitting, but this is enough given the price.
This review is about item#08745816.
Moisture removal
2
From Japan
On 2011-09-19 16:17:25
Evaluate that the water absorption is low, but the price is high. Because there are large arms and hem portions of the seams, products that are partially usable are mixed but judged to be price.
This review is about item#08745816.
Work to absorb oil leakage from the machine with waste.
1
From Japan
On 2008-10-15 09:53:44
As explained, I thought that it is not suitable for absorption of a large amount of oil because absorption is very bad. I think that it is good for work that wipes the dirt of the machine.
This review is about item#08745807.
1