Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of DDK05 Bushing with Brim

DDK05 Bushing with Brim
Sales Price: 2.99 SGD
Review Rating: 4.70
10 Customer Reviews
5 star 8
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
As a stopper
5
From Japan
On 2018-01-25 15:55:26
I bought it as a rotation stopper of a round bar This shape can not be found in the DY shop I stared from inside the catalog of Hattarou Because it is with a slide so it can correspond to dimensions in micron units so it is a very convenient product The field of vision has expanded
This review is about item#8751994.
Used for passenger mowers front wheels
5
From Japan
On 2017-07-31 07:13:20
The price is cheaper than the genuine product and the quality is equal and wonderful! I will continue to use it.
This review is about item#08751872.
Chillhole repair
5
From Japan
On 2017-06-08 15:37:50
Bush of the axis of Chillhole t - 16 flew away {made of plastic like plastic}} If you were looking for it, there was something just right and the installation went well.
This review is about item#8752064.
As a spacer
5
From Japan
On 2017-05-19 01:35:03
I tried using it as a spacer in the hole of the bell housing through which the clutch wire cable passes. The rattling disappears, it is a very good feeling.
This review is about item#08751574.
Motorcycle Maintenance
4
From Japan
On 2017-04-13 09:43:47
I am using it as a plastic replacement but it is in good condition! However ... because it is used in places where exchange frequency is high, if only a little cheaper. . .
This review is about item#8751391.
Repair of car body side hole of moped center stand
5
From Japan
On 2017-03-22 07:58:07
It repaired with bush because the body side hole of center stand spread. The play of the center stand got lost and it became very smooth.
This review is about item#08751495.
Ball bearing for turntable
5
From Japan
On 2017-02-27 19:57:53
DDK 05 Bush with collar OD and round washer Special size (stainless steel) 44.0 + 0.5 Inner diameter is perfect
This review is about item#8752317.
Factory equipment
3
From Japan
On 2016-02-25 17:59:18
I am satisfied that it was delivered smoothly because it was a customer's designated item.
This review is about item#08752134.
Repair and improvement of reels
5
From Japan
On 2015-08-17 19:57:24
It is used for repairing reels. There is no ball bearing that fits just the size, but since we need a slide at the operating point of the bail, we used it here. Although it seemed to be somewhat stuck before use, it started to move very smoothly after using it. In the list and individual item columns, the order code K5F0305-7 is also written as 3 mm in length, but from the relationship between model number and length, is not K5F0305-7 a product with a length of 5 mm? I think that it is a typographical mistake, but because it is a notation, both products are confused because they are products with a length of 3 mm. Please correct the notation. I am sorry if my misunderstandings are not written mistakes.
This review is about item#08751321.
Bearing looseness
5
From Japan
On 2013-12-18 00:37:06
Because there is no bearing fitting to the shaft, I searched for a bush with a flange with DDK 05. It was perfect for the size of the bearings you wanted to use.
This review is about item#08751434.
1
Customer Who Viewed This Item Also Viewed
Drymet LF Bush
DDK05 Thrust Washer
OILES #80 Bushing
Drymet Lf, T0.5
DDK05 Bush
Shell Type Needle Roller Bearing TA, Meter
Collared Bush
OILES No.300 Bushing