Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Heat Resistant Polyethylene Ball, Toilet

Heat Resistant Polyethylene Ball, Toilet
Sales Price: 10.99 SGD
Review Rating: 4.25
4 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Repair of ball tap of solar water heater
2
From Japan
On 2016-10-04 07:34:35
Polyball of a water tap ball tap manufactured about 20 years ago was destroyed and it began to overflow, so it was used for pol ball substitution. It is a water heater with hot water reaching 65 ℃, but it was not equipped with ball tap of heat-resistant polyballs, I checked that the screw of the pol ball be M6, but I did not find it. Although it is best to replace with a heat resistant ball tap, only pol balls are exchanged considering aged deterioration of each part. Would you remodel the arm or remodel the polka ball? Finally, I decided to retrofit the screw holes of the poly balls to 5.1 mm and make it to M6 screw processing. I made a hole with a drill and made screw machining of M6, but I managed to fix the arm somehow. Would you like to establish a M6 specification of a heat resistant polyball? I would like you to sell an unusual thread size such as using screws on both ends for M6 on both ends and W3 / 16 on the other.
This review is about item#34910041.
Repair
5
From Japan
On 2016-08-07 09:43:45
cheap. Of course there is no problem of quality.
This review is about item#34910041.
Solar bath
5
From Japan
On 2015-08-27 22:14:05
Although it is currently progressive type, the one we have been acquiring from the beginning, water has been submerged in the poly sphere though it has not uncovered a hole unexpectedly, if you are searching with monotaro you know the heat resistant poly sphere ordered It will be carried, probably, I think that I can go with it, there are stainless steel and copper balls, but it is saved because it is cheap
This review is about item#34910075.
Exchange float of water heater
5
From Japan
On 2013-03-04 21:12:44
I do not know if this has the meaning of a review, but it is a very genuine replacement part.
This review is about item#34910041.
1
Customer Who Viewed This Item Also Viewed
Polyball (Mounting screw M8)
Arm (mounting screws W1 / 4)
Arm (mounting screws W3 / 16)
Arm with Nut
Stainless Steel Ball
Polyethylene Float Ball
Low tank poly ball set
Horizontal Stainless Steel Ball Tap
Float Valve
Ball Tap Arm
Floating set
浮玉 set B
Poly Ball Tap, Heat Resistant
18-8 popular shallow type horn kitchen pot
Garden UV cut parasol 200cm