Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Ace Ball Straight Type, Both Outer Screw Type, Handle Color Blue

Ace Ball Straight Type, Both Outer Screw Type, Handle Color Blue
Sales Price: 11.99 SGD
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 1
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Attached to air compressor
4
From Japan
On 2018-04-14 01:09:15
Building was good. I wish I could turn the knob and change the direction.
This review is about item#08754426.
Air compressor air vent valve
3
From Japan
On 2017-03-02 18:10:58
I used this manufacturer's size of this size in the past, but now the air leaks out of the ball inside. The pressure is at most 7k, but since the compressor is mixed with fine dust etc., it is managed by self-responsibility. I think that there is not this trouble as I think that there is not one in the case of gas in the original use
This review is about item#8754426.
Output cut of the compressor
5
From Japan
On 2015-12-07 14:45:37
I would like to explain the difference between the price of the orange knob and the price.
This review is about item#08754426.
Opening and closing of air hose
5
From Japan
On 2015-06-23 21:01:58
I have used similar products from before. This time it was on the catalog so I bought it. I am using it as comparable to conventional products.
This review is about item#08754426.
Stop of compressor air
5
From Japan
On 2015-04-20 08:55:48
Since the thing which used was air leaked, it is using without any problem exchanged.
This review is about item#08754426.
It is attached to the discharge side of the oil mist separator connected to the small compressor.
3
From Japan
On 2009-11-02 19:11:01
There is an inner diameter of 6 mm, but the exhalation side was not 6 mm. (The entrance side was 6 mm) When connecting the hose, air leaked, I was in trouble, but I noticed that the inside diameter was not 6 mm, expanded to 6 mm with a drill and the air leak ceased. I would like you to describe the information accurately. However, I think the point where colors can be chosen is very good. You can tell at a glance, such as when there are multiple pipes in a narrow space.
This review is about item#08754417.
1